Announcements

Learn how to optimise USB-C for your designs at 18 May's USB-C PD Webinar.
Click here to register.

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

XiLu_4121146
Level 3
Level 3

  Hi,Srinath S

                    I designed one IO board use CYUSB3014,the VDD and AVdd  need  1.2V.I use spx3819m5-1-2 chip apply 1.2V voltage and 500mA current.But after tested,I found that it didn't work.I use TLV62130RGT chip provide 1.2V 3A ,it work.I found that Icc need 200mA and Icc USB need 60mA on the datasheet.Is it static work power?

usb3.0外扩板-正面01-论坛.jpg 

双目3.0-CYUSB3014-0715.png

1 Solution
YiZ_31
Moderator
Moderator
Moderator
1000 replies posted 750 replies posted 500 replies posted

Hi,

The work current will not exceed the sum of Icc Core max and Icc USB max. It is the maximun value.

Regards,
Eddie

View solution in original post

0 Likes
3 Replies
YiZ_31
Moderator
Moderator
Moderator
1000 replies posted 750 replies posted 500 replies posted

Hi,

The work current will not exceed the sum of Icc Core max and Icc USB max. It is the maximun value.

Regards,
Eddie

0 Likes

Hi,EddieZ_31:

                              I have checked the power.The 1.2V net only have some cap and the chip.But they costed much power.The test current much bigger than the datasheet's work current.What may cause the big power?

Regards,

Xibao 

0 Likes

Hi,Eddie:

        I doubt the chip welding may cause some problem.I will do some test though some test board.

Regards,

Xibao

0 Likes