- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
I am using an FX3, still in the superspeed development kit. It is connected to an ADC and I can stream data from the ADC via the FX3 into a PC using GPIF_example 1 firmware, an all new state machine, and the CollectData PC Utility. To start the ADC, I did have to send out two 32 bit words to the ADC. These were coincidentally the same value, so I was able to load the data counter and then output this twice using DR_DATA with the correct timing within the GPIF II designer state machine.
However, this only allows me to use the ADC in its default mode, I actually need a different mode.
I now need to send more configuration words to the ADC. However, there only seems to be this one counter you can directly load in the GPIF II designer. How can I output other fixed words to configure the ADC before starting the streaming? I would appreciate a fully explicit answer, I am new to this. This may be related to the CY_U3P_PIB_GPIF_EGRESS_DATA(thread_number) macro to source data from registers or CyU3PGpifWriteDataWords() for sockets but can someone provide details of how these are used. How do I write data into these sources (presumably in the firmware) and then put them out on the data lines with GPIF II?
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
OK I am still really struggling with this. Is there a developer/consultant who could take on a design of a FX3 USB 3 interface, preferably in the UK for our convenience but worldwide as long as their english language is good? I have checked the Cypress Design Partners Program but I can't find anyone suitable. As a minimum you must understand in full detail the project above. Please contact me via david.cruickshank@metrosol.co.uk if you are interested.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content