I now want to copy the sensor configurations into the CX3 firmware. But the sensor configurations occupy 28kB space. And my code area and data area size is 180kB and 30kB repectively by default. The data area space is insufficient. So I want to adjust the code area size to 150kB and the data area size to 60kB. How can I achieve it?
Solved! Go to Solution.
Hello,
You need to make changes to fx3.ld file as well cyfxtx.c file in the project you are working on.
Path for fx3.ld file ..Cypress\EZ-USB FX3 SDK\1.3\fw_build\fx3_fw
Default
{
I-TCM : ORIGIN = 0x100 LENGTH = 0x3F00 // 15 KB I TCM Area
SYS_MEM : ORIGIN = 0x40003000 LENGTH = 0x2D000 // 180 KB Code Area
DATA : ORIGIN = 0x40030000 LENGTH = 0x8000 // 32 KB Data Area
}
Modifications in fx3.ld file
I-TCM : ORIGIN = 0x100 LENGTH = 0x3F00 // 15 KB Descriptor Area
SYS_MEM : ORIGIN = 0x40003000 LENGTH = 0x25800 // 150 KB Code Area
DATA : ORIGIN = 0x40028800 LENGTH = 0xF000 // 60 KB Data area (40003000+ 0x25800=0x40028800)
Modifications in cyfxtx.c file
#define CY_U3P_MEM_HEAP_BASE (0x40037800) // Heap base (0x40028800 + 0xF000 = 0x40037800)
#define CY_U3P_MEM_HEAP_SIZE (0x8000) // 32 KB Heap (not changed)
after these modifications the path to the new fx3.ld file need to be updated in the properties (attachment) and then build the project
Please find the modified fx3.ld file in the attachement (as per the requirements mentioned). I have tested this with gpiftousb example of SDK 1.3.4, the firmware is building successfully.
Regards,
Rashi
Below is my error log trace after I copy the sensor configurations into the CX3 firmware.
Hello,
You need to make changes to fx3.ld file as well cyfxtx.c file in the project you are working on.
Path for fx3.ld file ..Cypress\EZ-USB FX3 SDK\1.3\fw_build\fx3_fw
Default
{
I-TCM : ORIGIN = 0x100 LENGTH = 0x3F00 // 15 KB I TCM Area
SYS_MEM : ORIGIN = 0x40003000 LENGTH = 0x2D000 // 180 KB Code Area
DATA : ORIGIN = 0x40030000 LENGTH = 0x8000 // 32 KB Data Area
}
Modifications in fx3.ld file
I-TCM : ORIGIN = 0x100 LENGTH = 0x3F00 // 15 KB Descriptor Area
SYS_MEM : ORIGIN = 0x40003000 LENGTH = 0x25800 // 150 KB Code Area
DATA : ORIGIN = 0x40028800 LENGTH = 0xF000 // 60 KB Data area (40003000+ 0x25800=0x40028800)
Modifications in cyfxtx.c file
#define CY_U3P_MEM_HEAP_BASE (0x40037800) // Heap base (0x40028800 + 0xF000 = 0x40037800)
#define CY_U3P_MEM_HEAP_SIZE (0x8000) // 32 KB Heap (not changed)
after these modifications the path to the new fx3.ld file need to be updated in the properties (attachment) and then build the project
Please find the modified fx3.ld file in the attachement (as per the requirements mentioned). I have tested this with gpiftousb example of SDK 1.3.4, the firmware is building successfully.
Regards,
Rashi