- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
They are thinking that interlaced design based on AN75779. And, they would like to confirm that the following specifications are feasible.
However, the project of AN75779 does not include the project created by CX3 Configuration.
[Spec]
MIPI : 148.5MHz 2lane
H-Active、 38.79us (38.79usx148.5MHz/4= 1440pix)
H-Blanking、 24.77us (=63.56us-38.79us)
V-Active、 odd/even:243/242
V-Blanking、 20/21 (or 19.5/20.5?) ?
Frame Rate、 30fps
THS-Prepare、~100ns
THS-Zero ~250ns
Q)
Why AN75779 did not include the CX3 configuration project, is there any reason for that?
Assuming that using only conformance is checked with CX3 Configuration, Is it feasible to apply the settings to cyfxuvcdscr.c directly to reflect the actual FW?
Best Regards
Arai
Solved! Go to Solution.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
In case the customer uses CX3, they can refer to OV5640 or AS0260 project in the FX3 SDK.
AN75779 is implemented for FX3.
Best regards,
Hirotaka Takayama
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
In case the customer uses CX3, they can refer to OV5640 or AS0260 project in the FX3 SDK.
AN75779 is implemented for FX3.
Best regards,
Hirotaka Takayama
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
In addition, AN90369 is helpful for the beginner of CX3 as well as UVC.