- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
I'm trying to get a system based upon AN75779 to work. I'm running under Linux (kernel 4.12.5).
When I run
v4l2grab -m -q 100 -d /dev/video0 -o /tmp/grab.jpg
When I run v4l2grab I get the following output
Image width set to 1280 by device /dev/video0.
Image height set to 720 by device /dev/video0.
and then it just hangs.
On my FX3 console I observe that streaming is activated when I start v4l2grab
UVC: Completed 0 frames and 0 buffers
UVC: Completed 0 frames and 0 buffers
UVC: Completed 0 frames and 0 buffers
UVC: Completed 21 frames and 3 buffers
UVC: Completed 42 frames and 19 buffers
UVC: Completed 63 frames and 35 buffers
UVC: Completed 84 frames and 51 buffers
UVC: Completed 106 frames and 9 buffers
However, in the Linux host kernel log I observe:
[ 7446.534814] uvcvideo: Found UVC 1.00 device FX3 (04b4:00f9)
[ 7446.536477] uvcvideo 2-6:1.0: Entity type for entity Extension 3 was not initialized!
[ 7446.536482] uvcvideo 2-6:1.0: Entity type for entity Processing 2 was not initialized!
[ 7446.536485] uvcvideo 2-6:1.0: Entity type for entity Camera 1 was not initialized!
[ 7446.536654] input: FX3 as /devices/pci0000:00/0000:00:14.0/usb2/2-6/2-6:1.0/input/input13
[ 8488.136849] uvcvideo: Failed to query (GET_DEF) UVC control 2 on unit 2: 1 (exp. 2).
What is the error "Failed to query (GET_DEF) UVC control" caused by?
v4l2grab works fine if plug in a plain USB web camera.
Solved! Go to Solution.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
The v4l2grab hang was due to a format error. Running mplayer revealed that there were only half of the expected pixels being output:
Frame too small! (921600<1843200) Wrong format?
After adjusting the YCbCr format mplayer now runs without the above, and v4l2grab will complete with the grabbed image.
The "Failed to query" kernel message is still there, but it does not seem to be fatal.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
The v4l2grab hang was due to a format error. Running mplayer revealed that there were only half of the expected pixels being output:
Frame too small! (921600<1843200) Wrong format?
After adjusting the YCbCr format mplayer now runs without the above, and v4l2grab will complete with the grabbed image.
The "Failed to query" kernel message is still there, but it does not seem to be fatal.