Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

USB superspeed peripherals

liuzq
Level 1
50 sign-ins 25 sign-ins 10 replies posted
Level 1

cypress专家您好,

  使用FPGA+cyusb3014实现UVC+UART,就是FPGA在不断发送给cyusb3014视频的同时,上位机可以向FPGA发送控制字,FPGA收到控制字后要向上位机返回结果,两个通道互不相影响。

请教两个问题:

1),FPGA和cyusb3014具体怎样连接?

2),FPGA应该怎样向 cyusb3014发送数据才能做到两个过程互不相影响?

谢谢

0 Likes
1 Solution
YiZ_31
Moderator
Moderator 1000 replies posted 750 replies posted 500 replies posted
Moderator

这个上位机向FX3发送自定义控制字有很多方法,不一定需要添加uart接口,比如通过UVC extension unit

https://community.cypress.com/t5/Knowledge-Base-Articles/FX3-CX3-UVC-Extension-Unit-Application-KBA2...

添加串口的教学:

https://community.cypress.com/t5/Knowledge-Base-Articles/Adding-Communication-Device-Class-Interface...

这里是把USB接收到的串口消息直接通过FX3的 uart口传了出去,你要是想用别的如I2C也可以。

具体如何连接请参考AN75779中的内容:

https://www.cypress.com/documentation/application-notes/an75779-how-implement-image-sensor-interface...

View solution in original post

0 Likes
7 Replies
YiZ_31
Moderator
Moderator 1000 replies posted 750 replies posted 500 replies posted
Moderator

这个上位机向FX3发送自定义控制字有很多方法,不一定需要添加uart接口,比如通过UVC extension unit

https://community.cypress.com/t5/Knowledge-Base-Articles/FX3-CX3-UVC-Extension-Unit-Application-KBA2...

添加串口的教学:

https://community.cypress.com/t5/Knowledge-Base-Articles/Adding-Communication-Device-Class-Interface...

这里是把USB接收到的串口消息直接通过FX3的 uart口传了出去,你要是想用别的如I2C也可以。

具体如何连接请参考AN75779中的内容:

https://www.cypress.com/documentation/application-notes/an75779-how-implement-image-sensor-interface...

0 Likes
liuzq
Level 1
50 sign-ins 25 sign-ins 10 replies posted
Level 1

liuzq_0-1617174864731.png

在AN75779里是这样描述FX3和CMOS图像传感器之间的管脚连接的,其中LV,FV,GPIO[0:7},PCLK这些管脚是用于传输数据用的,而I2C_GPIO[58],I2C_GPIO[59]只是用于控制CMOS图像传感器的,也可以省略,对不对?  FX3与FPGA的连接也是同样的对么?FPGA与FX3之间要实现双通道(图像数据通道与控制命令通道分开)也是通过FX3的外设(UART,I2C,SPI)管脚与FPGA物理连接实现的,对么?(原来以为图像数据和控制命令都是通过GPIF II发送,接收的),谢谢

0 Likes
YiZ_31
Moderator
Moderator 1000 replies posted 750 replies posted 500 replies posted
Moderator

控制和数据当然是分开的,GPIF只负责接受图像数据。无论你用什么方法,只要保证GPIF接收到正确的图像数据。这行场信号同步不是我们家定义的,很多地方都用。

 
0 Likes
liuzq
Level 1
50 sign-ins 25 sign-ins 10 replies posted
Level 1

FPGA通过GPIF II方式(非Slave Fifo Synchronize模式)读写FX3的verilog HDL例程有么?网上只能找到slavefifosync模式的例程。谢谢

0 Likes
YiZ_31
Moderator
Moderator 1000 replies posted 750 replies posted 500 replies posted
Moderator

没有。GPIF是我们这个接口的名称,这个状态机是可以用GPIF II designer自己设计的,与FPGA匹配即可。slave fifo只是其中一个例程的名字。

0 Likes
liuzq
Level 1
50 sign-ins 25 sign-ins 10 replies posted
Level 1

liuzq_0-1617248385134.png

 

FPGA按AN75779的GPIF II模式()如上图)读写FX3时,向FX3提供的PCLK脚的时钟频率应该是多少(是<=100MHz么?)?我有一块Xilinx Zc702的开发板,它的D18,C19脚输出一对200MHz的差分时钟,可以分频后用于FX3

0 Likes