windows 7 driver - cy7c68013a

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
Anonymous
Not applicable

I need driver for windows 7 for device cy7c68013a-56pvxc.

   

Is there driver for this device?

0 Likes
71 Replies
Anonymous
Not applicable

After installing SuiteUSB 3.4 - USB Development Tools for Visual Studio, you can find the CYUSB.sys driver in the below directory.

C:\Program Files\Cypress\Cypress Suite USB 3.4.1\Driver

This driver supports 32 bit and 64 bit versions of Windows XP,Windows Vista and Windows 7.

   

For windows 7 you will find in the C:\Program Files\Cypress\Cypress Suite USB 3.4.1\Driver\wlh

0 Likes
Anonymous
Not applicable

Hello

   

I wanted to use this driver , win 7 but said there was no driver in this directory

   

I modified the. inf file to vid to 04b4 and pid to 8613

   

regards

0 Likes
lock attach
Attachments are accessible only for community members.
Anonymous
Not applicable

Hi ,

   

You need to edit the file in the directory where your driver is , i.e. suppose you sre using win7 32 bit then this is the path "C:\Program Files\Cypress\Cypress Suite USB 3.4.2\Driver\bin\wlh\x86" if you are using win7 64 bit then "C:\Program Files\Cypress\Cypress Suite USB 3.4.2\Driver\bin\wlh\x64", both these folders have inf files depending upon your OS add the vid/pid info in the correct inf file and point to it when asked for driver.

   

I am attaching a inf file for 64bit win 7 , if you want for 32bit then modify the vid pid under ;for x86 platforms.

   

-shubham

0 Likes
Anonymous
Not applicable

Thank you for the answer
I edit the file and I tried the x64 version and x86

   

but Windows 7 said he does not find a driver in this directory
I did the test without the jumper with VID 04b4 and PID 8613
with jumper the vid/pid is 0925 and  3881

   

What is the problem ?

   

Laurent F4FDW

0 Likes
Anonymous
Not applicable

您好

   

我用上述的方法做过了,可是不可以实现,在xp系统下可以用,但是在win7下找不到设备

   

希望能给我点建议

   

谢谢

0 Likes
Anonymous
Not applicable

hello

   

i have done by your process in win7 ,but the computer said unkonw device.......

   

so can you give me some advice

   

thanks

0 Likes
Anonymous
Not applicable

Hi Pitt,

   

What is the exact error message you're seeing?

   

Regards,

   

Anand

0 Likes
Anonymous
Not applicable

I have the same problem; if it’s like my case he gets the very descriptive message:

   

“Windows could not find driver for your device.”

   

 

   

My thread is: http://www.cypress.com/?app=forum&id=167&rID=50852

0 Likes
Anonymous
Not applicable

I have the same problem with window 7 x 64

   

the usb driver is not loading

   

got your copy of cyusb1.inf

   

pointed back to this file to install the driver .

   

Windows has stopped this device because it has reported problems. (Code 43)

   

when i try to update the driver windows comes back with a message

   

 

   

 

   

"windows has determined the driver software for your device is up to date"

   

Unknown Device

   

 

   

if i click on driver details i get

   

" no driver files are required or have been loaded for this drvice"

   

I am stuck now cant get this to work is there any other way to get the driver to load?

   

M0DMJ

0 Likes
lock attach
Attachments are accessible only for community members.
Anonymous
Not applicable

Hello,

   

I've tried everything, but I can´t get it work. Right now, I get that the driver has been found and it's instaled,  but Windows stopped him.

Erorr code 10.

I have been trying to start my developement for about 10 days 😞 I'm stuck !!


regards

0 Likes
Anonymous
Not applicable

M0DMJ,

   

In cyusb1.inf there is a ; before the VID_04B4 statement. ; is a comment line in inf file. Remove that ; and modify the corresponding lines to your VID/PID and it should work fine.

   

Regards,

   

Anand

0 Likes
Anonymous
Not applicable

Gonmalo,

   

Are you using the board with a firmware? if so which firmware?

   

Regards,

   

Anand

0 Likes
Anonymous
Not applicable

Hi,

   

of course I made all the modifications to the .inf file to get to this point. I don't know wich firmware, I'm trying to connect to the chip for the first time.

   

 

   

greetings

0 Likes
Anonymous
Not applicable

Gonmalo,

   

Are you using FX2LP DVK (CY3684) or a custom  board. What is the VID/PID being displayed in device manager for the device?

   

Regards,

   

Anand

0 Likes
Anonymous
Not applicable
0 Likes
Anonymous
Not applicable

Hi    🙂

   

 

   

maybe it's a good idea to delete my posts. But maybe it's a better idea keep them, for someone who could be as unlucky as me!!

   

Always check on your USB cable, this was the problem 😞 I changed it for a new cable and ... perfect it worfs perfect.

   

 

   

PS: its a custom board, that I bougth in China

   

 

   

 

   

regards

0 Likes
Anonymous
Not applicable

I have a board with CY7C6013A. When I plug into my PC Window 7 , PC  always try to install the driver for my previoues installed driver for AN2131SC.   Is there anyway to install the new driver ?

0 Likes
Anonymous
Not applicable

Are you using Windows 7 32-bit or 64-bit OS? Is your driver for AN2131SC a signed driver?

   

Regards,

   

Anand

0 Likes
hahac_299066
Level 1
Level 1

my pc is win7 64bit 128pinCY7c68013 can be use ,but 64pin CY7c68013 can be used and is a "Unknown Device"

   

I want to know why,how can I deal with this problem.

0 Likes
Anonymous
Not applicable

 Hello Sciencefuture,

   

 

   

I could not understand your exact problem. Can you detail the same.

   

 

   

Regards,

   

Gayathri

0 Likes
zeLu_283996
Level 2
Level 2
First like given

I bought a cy3864 advanced development board, try work in windows 7 64bits system,but can not solve the driver problem, can not find it anywhere i tried.

   

help

0 Likes
Anonymous
Not applicable

 http://www.cypress.com/?id=4&rID=53338

   

Cheers,

   

Anand

0 Likes
zeLu_283996
Level 2
Level 2
First like given

same problem.

   

edit cyusb.inf in  ulh/x64, modyfied vid&pid, uncommoned. copy to windows/inf

   

copy cyusb.sys to windows/system32/driver

   

 

   

system say 'conn't find corresponding file

   

 

   

I used 3864 develop ezusb deve kit

0 Likes
zeLu_283996
Level 2
Level 2
First like given

system said:

   

Windows found driver software of your device but encountered an error attempting to install it.

   

Cypress USB generic driver (3.4.7.000)

   

the system connot find the file specified.

0 Likes
Anonymous
Not applicable

 That is because the inf file will say the driver is in the same folder as the driver file. Don't do the copying.

   

Keep both inf file and driver file in same folder and try.

   

 

   

Only if you use a installer it will take care of specifying the drivers are in the specific system tolder.

   

Regards,

   

Anand

0 Likes
zeLu_283996
Level 2
Level 2
First like given

solved thanks.

0 Likes
Anonymous
Not applicable

I'm using window 7, 64xbit operating system.  I have inserted the following and still it did not work.

   

 

   

;for x86 platforms
[Device.NTx86]
VID_04B4&PID_8613.DeviceDesc%=CyUsb, USB\VID_04B4&PID_8613

   

;DMM measurement

   

VID_0F22&PID_F020.DeviceDesc%=CyUsb, USB\VID_0F22&PID_F020

0 Likes
lock attach
Attachments are accessible only for community members.
Anonymous
Not applicable

 Hi,

   

 

   

[Device.NTx86] is for 32 bit processor. Since yours is a 64bit systems, you need to write the VID/PID under [Device.NTamd64]. Please find attached inf file. I have added the two entries for you in the appropriate section. Please check it out. 

   

 

   

Regards,

   

Gayathri

0 Likes
lock attach
Attachments are accessible only for community members.
Anonymous
Not applicable

Thanks, I tried that and it does allow to me to install without digital signature, but my device manager still show the yellow exclaimation mark

   

for x64 platforms
[Device.NTamd64]
;VID_XXXX&PID_XXXX.DeviceDesc%=CyUsb, USB\VID_XXXX&PID_XXXX
VID_04B4&PID_8613.DeviceDesc%=CyUsb, USB\VID_04B4&PID_8613

   

; DMM
VID_0F3F&PID_F010.DeviceDesc%=CyUsb, USB\VID_0F3F&PID_F010

   

; Scope
VID_0F3F&PID_F022.DeviceDesc%=CyUsb, USB\VID_0F3F&PID_F022

   

 

   

Pleas advise,

   

 

   

thanks

0 Likes
Anonymous
Not applicable

 Hi,

   

 

   

In the entries that you have posted in the previous response, I see % symbol missing at the very start of the entry. It should be as below:

   

   

%VID_0F3F&PID_F010.DeviceDesc%=CyUsb, USB\VID_0F3F&PID_F010

I believe you missed that thing only in the post. Please ensure the same.   

   

 

   

When you are binding using the Install driver Wizard, what does it show at the end? Does it give some warning/ error message ? Please check VID/PID being shown in the Device manager (right click on device -> Properties -> Details tab). Also check what is the message displayed in the Device Status coloumn in the Device manager (right click on device -> properties -> General tab). Please attach screenshots of both.

   

Did you use the same inf file that I had attached in the previous response? Just change its to CyUSB.inf (change extension from txt to inf). Just wanted to ensure this.

   

 

   

Regards,

   

Gayathri

0 Likes
lock attach
Attachments are accessible only for community members.
Anonymous
Not applicable

I tried on my other Win7, AMD processor, 32-bit operating system. device driver installed succesfully.  However, I would like to have it work on Win7, Intel processor, 64-bit operating system.  Attached are the snapshots after implementing changes per your advice.

   

 

   

Thanks
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
[Device.NTamd64] is meant for 64-bit processors with architecture other than intel itanium architecture. So, it should be [Device.NTia64] is for Intel itanium architecture processors. Please make the change in the inf and try.

   

 

   

Regards,

   

Gayathri

0 Likes
Anonymous
Not applicable

Hi,

   

 

   

thanks for your tremendous help. Please see the attached inf file. I have modified .inf file to work with intel 64xbit, window 7 operating system and it still did not work.  Please advise if you find out something within the code.

   

 

   

thanks again,

   

TuDo

0 Likes
Anonymous
Not applicable

Hi,

   

       Attachment is missing.

0 Likes
Anonymous
Not applicable
0 Likes
Anonymous
Not applicable

Sorry, here is the attachement.

0 Likes
lock attach
Attachments are accessible only for community members.
Anonymous
Not applicable

Wow...sorry, I forgot to change .inf to .txt

   

 

   

thanks

   

Tudo

0 Likes