- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello,
I have interfaced image sensor to fx2lp in slavefifo mode and for this,i have modified control center to display the image in the pc side.image sensor is 752x480 resolution with 60 frames per second.what ever the image frame is displaying in the pc is shifting,that means first frame(partial) is displaying with second frame(partial) in the dispaly.
why it is happening?is it because of data loss?fx2lp and windows are not in sync?how can i solve this problem?i have attached the image display.
help me.
Solved! Go to Solution.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello Geethanjali,
The data is read from the device by the host application using the XferData() API. This API stores the data onto a buffer. Kindly, implement the comparison on the data received on the buffer.
Best regards,
Srinath S
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
Can you please compare the frame which is sent into PC and the frame which is displayed on the app?
1) Use a protocol analyzer like USBLyzer and get the data of one single frame
2) Get the data of one single frame as seen by the host application, right before it is sent for display
Compare the two data. If they are same, then the problem is not with the PC/App side. It could be with the image sensor / fpga / fx2lp.
If not, the issue is with the host application code.
Regards,
- Madhu
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi sir,
we dont have USBLyzer,any other debug process.
thanks for your replay.
regards,
geethanjali.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
USBLyzer is a software analyzer. You don't need any other hardware. Download it from here:
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi Madhu,
THANK YOU.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi madhu,
Compare the two data. If they are same, then the problem is not with the PC/App side. It could be with the image sensor / fpga / fx2lp.
If not, the issue is with the host application code.
-->two data are different,see the usbanalyser screenshot,what whould be control center problem?
image sensor is 752x480 resoltion ,60 frames per second.For every transaction,i am getting 360960bytes.
How can i solve this?
regards,
geethanjali.
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
Hello Geethanjali,
The start of a new frame has to be identified by the host application. This can be done by generating a known byte header pattern in the FX2LP firmware and looking for the same in the host application.
Best regards,
Srinath S
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello,
we are implemented header pattern in both host application and fx2lp.we are adding a known 8 bytes of data when frame valid goes low,same 8 bytes are recieving in the host application.between these successive headers there is a 360960+512 bytes.360960 bytes are complete one frame according to image sensor datasheet.but when i look into the one frame,frame is splitted as shown in the image file.
what would be the reason?
regards,
geethanjali.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello,
The start of a new frame has to be identified by the host application. This can be done by generating a known byte header pattern in the FX2LP firmware and looking for the same in the host application.
->
we are added 8 bytes of data,that is header in the fx2lp and this is confirmed with default control center.but we are unable to looking for this header in the control center host application.where i can get this string in the host control center application?how can i compare this header in the host side code?can anyone tell me the where should look into the code?
regards,
geethanjali.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello Geethanjali,
The data is read from the device by the host application using the XferData() API. This API stores the data onto a buffer. Kindly, implement the comparison on the data received on the buffer.
Best regards,
Srinath S