Announcements

Learn how to optimise USB-C for your designs at 18 May's USB-C PD Webinar.
Click here to register.

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Anonymous
Not applicable

 Hi 

   

I am trying to define the EP8 as out in my FX2 (using the slave fifo)

   

but when i send from the host block to EP8 the 'get config desc' hangs and the software is stuck.

   

if i no write to EP8 it works. 

   

here is the code

   

 

   

   

void TD_Init(void)             // Called once at startup

   

{

   

 

   

  REVCTL = 0x03; // MUST set REVCTL.0 and REVCTL.1 to 1

   

   

IFCONFIG = 0x43; // use IFCLK pin driven by external logic (5MHz to 48MHz) slave fifo

   

// use slave FIFO interface pins driven sync by external master

   

SYNCDELAY;

   

 

   

 

   

SYNCDELAY;

   

EP2CFG = 0xEA; // sets EP2 valid for IN's  triple(x2) buffer, size 512, bulk

   

 

   

SYNCDELAY;

   

// EP4CFG = 0xE0; // sets EP4 not valid (ep2) for out, bulk

   

EP4CFG = 0x00;

   

 

   

SYNCDELAY;

   

// EP6CFG = 0xE0; // sets EP6 valid for IN's, bulk, 512 double

   

EP6CFG = 0x00;

   

 

   

SYNCDELAY;

   

EP8CFG = 0xA0; // sets EP8 valid for OUT 's , bulk

   

 

   

 

   

SYNCDELAY;

   

   

SYNCDELAY;

   

  FIFORESET = 0x80; // reset all FIFOs

   

SYNCDELAY;

   

FIFORESET = 0x02;

   

SYNCDELAY;

   

FIFORESET = 0x04;

   

SYNCDELAY;

   

FIFORESET = 0x06;

   

SYNCDELAY;

   

FIFORESET = 0x08;

   

SYNCDELAY;

   

FIFORESET = 0x00;

   

SYNCDELAY; // this defines the external interface to be the following:

   

SYNCDELAY;

   

EP2FIFOCFG = 0x0D; // this lets the FX2 auto commit IN packets, gives the //8bit

   

SYNCDELAY;

   

SYNCDELAY;

   

EP4FIFOCFG = 0x05; // this lets the FX2 auto commit IN packets, gives the//8bit

   

SYNCDELAY;

   

SYNCDELAY;

   

SYNCDELAY;

   

EP6FIFOCFG = 0x00; // this lets the FX2 auto commit IN packets, gives the//8bit

   

SYNCDELAY;

   

SYNCDELAY;

   

EP8FIFOCFG = 0x00; // this lets the FX2 auto commit IN packets, gives the//8bit

   

SYNCDELAY;

   

// ability to send zero length packets,

   

// and sets the slave FIFO data interface to 8-bits

   

SYNCDELAY;

   

 

   

SYNCDELAY;

   

OUTPKTEND = 0x88; // Arm both EP2 buffers to “prime the pump”

   

SYNCDELAY;

   

OUTPKTEND = 0x88;

   

 

   

// and defines the endpoint for 512 byte packets, 2x buffered

   

PINFLAGSAB = 0x00; // defines FLAGA as prog-level flag, pointed to by FIFOADR[1:0]

   

SYNCDELAY; // FLAGB as full flag, as pointed to by FIFOADR[1:0]

   

PINFLAGSCD = 0x00; // FLAGC as empty flag, as pointed to by FIFOADR[1:0]

   

 

   

FIFOPINPOLAR = 0x00; // set all slave FIFO interface pins as active low

   

 

   

 

   

 

   

EP2AUTOINLENH = 0x02; // you can define these as you wish,

   

SYNCDELAY; // to have the FX2 automatically limit IN's

   

EP2AUTOINLENL = 0x00;

   

SYNCDELAY;

   

 

   

// EP8AUTOINLENH = 0x02; // you can define these as you wish,

   

// SYNCDELAY; // to have the FX2 automatically limit IN's

   

// EP8AUTOINLENL = 0x00;

   

// SYNCDELAY; // out endpoints do not POR (power-on reset) armed

   

 

   

// SYNCDELAY; // out endpoints do not POR (power-on reset) armed

   

 

   

   // Set the fifo programmable level of EP2

   

   // Set level to 3 packtes  +  1024*3+992 = 4064 (out of 4096)

   

  /* EP2FIFOPFH = 0x1B;

   

   SYNCDELAY; 

   

   EP2FIFOPFL = 0xe0;  */

   

   

EP2FIFOPFH = 0x0B;

   

    SYNCDELAY; 

   

    EP2FIFOPFL = 0xE0;   

   

 

   

 

   

SYNCDELAY; 

   

SYNCDELAY; 

   

 

   

 

   

    EP1OUTCFG =0xA0;

   

    EP1INCFG  =0xA0;

   

SYNCDELAY; // out endpoints do not POR (power-on reset) armed

   

   

 

   

   EP1OUTBC = 0x40;              // arm ep1out (warning: only 64 bytes deep)

   

   EP1INBC = 0x40;              // arm ep1out (warning: only 64 bytes deep)

   

}

1 Reply
Anonymous
Not applicable

  Hi,

   

  The buffer configuration that you have used is invalid, please go through section 1.17 EZ-USB Endpoint Buffers of TRM for valid buffer configurations.

   

    For a bulk endpoint the FIFO buffer size needs to be set to 512  bytes and not 1024 bytes. As per  USB 2.0 spec the  maximum packet size of a bulk endpoint is restricted to 512 bytes and  the data is transferred over USB in packets of 512 bytes maximum.  So, in order to maintain  conformity, the endpoint size in the FX2LP must be configured for 512  bytes, please look into EP2 buffer configuration

   

 

   

Thanks 

   

   

Prajith

0 Likes