Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

USB low-full-high speed peripherals Forum Discussions

Anonymous
Not applicable

Hi, I am trying to use CY7C68013A to transfer data from Sensor to PC. 

   

I use EP2 on slave FIFO mode.The FIFO is 512x4.My PC is programmed by VC++ 2012, using the function BeginDataXfer,WaitForXfer and FinishDataXfer to receive 1 frame per cycle.My driver is cyusb3.sys.

   

When my OS is win7,i can get data.

   

But in XP,when the Xfer length is lager than 3840000bytes,the system die,and i have to Forced shutdown.and when length is 3520000 or less,it can get data.

   

Then i use USB Control Center:Transfer Data-IN,it is the same.The WIN7 is OK,but XP die...(when Bytes to Transfer is 3840000)

   

So,what is the problem?OS?

0 Likes
1 Reply
Anonymous
Not applicable

https://msdn.microsoft.com/en-us/library/ff538112.aspx

   

i think the ans is this...

   

bulk:win7 4MB for high and full speed

   

        xp    3MB for high and full speed

   

 

   

but in win7,when transfer size>4M,it can auto separate to 4M+the rest size.

   

in xp,when transfer size>3M,the system die...      

0 Likes