- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi, I am trying to use CY7C68013A to transfer data from Sensor to PC.
I use EP2 on slave FIFO mode.The FIFO is 512x4.My PC is programmed by VC++ 2012, using the function BeginDataXfer,WaitForXfer and FinishDataXfer to receive 1 frame per cycle.My driver is cyusb3.sys.
When my OS is win7,i can get data.
But in XP,when the Xfer length is lager than 3840000bytes,the system die,and i have to Forced shutdown.and when length is 3520000 or less,it can get data.
Then i use USB Control Center:Transfer Data-IN,it is the same.The WIN7 is OK,but XP die...(when Bytes to Transfer is 3840000)
So,what is the problem?OS?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
https://msdn.microsoft.com/en-us/library/ff538112.aspx
i think the ans is this...
bulk:win7 4MB for high and full speed
xp 3MB for high and full speed
but in win7,when transfer size>4M,it can auto separate to 4M+the rest size.
in xp,when transfer size>3M,the system die...