- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
I tried the cy3684 kit's example, when I test the vendor command I found a problem:
I use the large eeprom 24lc128 (128kbit or 16kbyte), I use vendor command "A9" "Out" mode to write "11 11 11 ....."(64 in total) to address started from 0x3FC0 (the xValue I put into the cy console software interface), it works.
But when I change the xValue to 0xFFFF and write another one "11" (only 1 byte), it works too after I recycled the power, the "11" content at 0xFFFF still exists!
the 24lc128 only has 0x0-0x3FFF address range, where does the xValue=0xFFFF locate at?
I am confused.
- Labels:
-
ispn:39563:1:0
-
l1:314:1:0
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
This should not happen with the vend_ax example code.
Maybe there is an older version of the code that is circling the address back to the nearest/next valid address.
Please create a support case on our website if this issue still exists.