Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

USB low-full-high speed peripherals Forum Discussions

Sort by:
nguyenlong
USB low-full-high speed peripherals
I have a folder driver for printer which is used for win 10 (intel) and they include 3 files: cyusb3.sys, cyusb3.cat, cyusb3.inf. I tried to install t... Show More
Tony-Zhang
USB low-full-high speed peripherals
Dear Friend I want to build a data acquisition board with a FPGA sending data to PC via USB port.   I think CY7C68015A/CY7C68016A is a good choice for... Show More
dennishsu_xu
USB low-full-high speed peripherals

请问下 CY7C68013A怎样配置USB进入test packet mode 以测试USB信号眼图一致性?有没有具体的寄存器配置指导?

myzxc
USB low-full-high speed peripherals
Hello, I would like to ask what is the maximum sampling period for reading sensor data with cy7c65211A chip as the master and the corresponding sensor... Show More
Bill_H
USB low-full-high speed peripherals

Need download link for SuiteUSB, has it been obsoleted? If yes, what is its replacement?

Allenyyj
USB low-full-high speed peripherals
Hi, I'm using Cypress 68013 to transfer the data from Medical Device EEG amplifier to computer with high-speed USB. When transferring, there is a high... Show More
jeidi98
USB low-full-high speed peripherals
Hello,While using a board using a cyusb3014 chip, I have a question about the debug interface in chapter 5.9, AN75779. In general use,When I download ... Show More
myzxc
USB low-full-high speed peripherals
Hello, I would like to ask how many slaves can be connected when the cy7c65211a chip uses SPI mode as the MASTER. Some of the data taken by my channel... Show More
barbeque
USB low-full-high speed peripherals
买了开发板想读取nand flash数据,但是不会使用。求助
wumj21
USB low-full-high speed peripherals
hi,    When I used AN8716 firmware to send a message from the slave device to the master device on the CYUSB3KIT003 development board, the... Show More
Forum Information

USB low-full-high speed peripherals

Discussion forum regarding USB low-full-high speed peripherals topics.