Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

USB low-full-high speed peripherals Forum Discussions

Sort by:
Ivan_Lee
USB low-full-high speed peripherals
I am try to modify inf file to add a new VID/PID .but it can't successfully to install driver.How to do? Show More
AaCl_287166
USB low-full-high speed peripherals
        Hello        I loaded a new *.iic File to the 24lc128 eeprom that we are using. In the software I changed some Registers settings and (that's ... Show More
siz
USB low-full-high speed peripherals
Hello, I write here because I am new to Cypress devices and I would like to clarify a few doubts.For a project I am working on I need to transfer (wit... Show More
user_4533981
USB low-full-high speed peripherals
When the official downloaded HID firmware instance runs, the device is identified as a keyboard. If I want it to be identified as a mouse, do I just n... Show More
faM_4540176
USB low-full-high speed peripherals
i bought a light engine and it consists of cypress dual channel module. i use raspbian stretch lite. the problem is that when i attach the device with... Show More
foho_4476016
USB low-full-high speed peripherals
Hey GuysI'm using CY7C68034 with two nand flashes, first i used "MT29F16G08FAA" from Micron, which i was not able to program using mfg tool, i could j... Show More
user_4533981
USB low-full-high speed peripherals
hello: 请问在Windows10下可以安装USB2.0驱动么?为什么HID的实例无法运行,且用烧录程序后,这样显示,能具体告知如何正确导入hid_kd程序么,如何让CY7C68013实现HID功能么?操作结果如附件:由于本人第一次开发CY7C68013的HID功能,请帮忙告知详细步骤谢谢。Ca... Show More
user_4533981
USB low-full-high speed peripherals

本人目前做CY7C68013开发,已下载官网开发包但缺少HID上位机控制程序,官网所提供的程序运行也有问题,能提供一份新的么?

chLi_4456426
USB low-full-high speed peripherals

hello

I want CyUsb3 Driver Resell,

INF and Driver info is refer to the attached file

hata_3396041
USB low-full-high speed peripherals
HelloPlease tell me about Initial settings of CY7C65211A.1.Is there a format for customers to list specifications? (If you have something like USB-PD)... Show More
Forum Information

USB low-full-high speed peripherals

Discussion forum regarding USB low-full-high speed peripherals topics.