USB low-full-high speed peripherals Forum Discussions
Hi there 😉
I have a DVB-s2 Tuner that needs to be connected to a Linux machine using the CY7C68013a FX2LP.
Interface from the demodulator is 8-Bit parallel TS transport stream.
There is also a serial TS interface but i guess thats too fast to capture.
On the Linux i guess its necessary to use libusb and write an application to read the data and control the channels.
The reference designs "CY_FX2LP_LGS_ DMB-TH_TV Dongle", there is a folder "firmware->USBTV".
is that for the CY7C68013a - chip? to be downloaded on connect?
What SDK do i need to compile this firmware?
I have just an CY7C68013a mini board.
Thanks!
Show LessWe are looking for an USB-to-JTAG bridge solution. The expected TCK of JTAG is 30MHz. Does Infineon(Cypress) have this solution?
We will use it to program FPGA/CPLD.
Regards,
Kyle
Show LessI need breakout USB to UART interface module based on CY7C65213A.Do you have, kindly let me know. Can you clarify that Is there any module with CY7C65213A.I have seen the USB UART Serial Breakout- CY7C65213 but it is not suitable for RS485.So I want USB UART Serial Breakout with CY7C65213A.
Can you tell me the hardware difference of both IC's. Do you have the USB UART CY7C65213A breakout
Show LessDear Sirs,
I would like to proceed with driver signing.
Attached there drivers with cat files signed with our EV Certificate by GlobalSign CA.
My company dashboard account is optikon2000@onmicrosoft.com
Regards,
Stefano
Show LessHello, I am using the CY7C65213-28PVXIT on my new PCB design. I want to configure the bridge for USB Bus Powered. I have looked on page 15 Figure 15 and would like to know it it is okay to filter the VBUS power that is connected to VCC and VCCIO?
Thank you
Joe
Show LessHi, I have an I/O box in my inspection machine that it used CY7C63743C-PXC as Low-Speed USB and PS/2 Peripheral Controller . It seems the I/O box is damaged and can’t communicate with PC and its USB port is unknown.
When the USB cable from this box connects to PC , this error message appears on the screen.
what do you think? what's the problem? Is there any drivers for this IC?
with regards
Bahar
Dear Sirs,
i would like to proceed with driver resell for CyUsb3 drivers.
I have
USB EV certificate from GlobalSign
By our company modified .Inf and .cat files
Microsoft Hardware Dashboard Publisher Display Name : admin@optikon2000@onmicrosoft.com
We would sign driver for Windows 10, Windows 8, Windows 8.1 both 32 and 64 bits.
Target device are Keratron family topographer equipped with Cy7C68013A chip.
Attached driver files.
Thahk you and best regards,
Stefano
Show LessCY7C65211A (CDC mode)can be conneted to Cypress USB-Serial Configuration Utility.
Modified it to Vendor mode ,USB Serial Test Utility can find it,but Cypress USB-Serial Configuration Utility not.
How can I configure CY7C65211A back to CDC mode? THKs!
Show Less
Hi,
This is Bhuvaneswari, I need to know few details listed for the Parts Mentioned below:
CYPD3176-24LQXQ
CY7C65211-24LTXI
Imformation Required:
1. Current status of the part.
2. If active, then how long it will be supported?
3. Is there any EOL issued for both parts?
4. Can u provide ROHS documents for both the parts?
Kindly consider this as priority and respond me as soon as possible.
Show Less