Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

USB low-full-high speed peripherals Forum Discussions

SaBh_294166
USB low-full-high speed peripherals
Hi. Trying to develop a new product based on the FX2LP so recently purchased the CY3684 kit. The docs appear to be out of sync with the current softwa... Show More
JeBo_4132831
USB low-full-high speed peripherals
Hi, Another day, another question ... 🙂 We are finalizing our Firmware. One question regarding the Descriptor Name. We want to display something like... Show More
amusz
USB low-full-high speed peripherals
Hi, We are wroing on a reference design using a PSoC 62 and a CY7C65215 as USB-UART bridge to debug. While usign the last one in bus powered mode we h... Show More
vpac
USB low-full-high speed peripherals
In my fx2lp-application the 8051-CPU collects data via interrupt and wants to write the bytes into EP2IN fifo. So..plain CPU driven EP2IN filling. I w... Show More
MichaelR
USB low-full-high speed peripherals
Dear Sir or Madam, Since I am neither a professional programmer nor a lawyer, I have a question regarding the license of the CyUSB.dll. I designed a c... Show More
KyUn_4602541
USB low-full-high speed peripherals
We are designing a board that we want to use with as many Android phones as possible.  What would be the most generic, widely support USB 2.0 chipset ... Show More
JeBo_4132831
USB low-full-high speed peripherals
Hi, I use the SlaveFIFO mode (in 16bits mode) to communicate with my FPGA. I use alos EP2 for OUT and EP6 for IN. The 4 flags are also used. I attache... Show More
MiRo_263836
USB low-full-high speed peripherals

Does Infineon offer any USB OTG devices?  It seems like USB OTG is not used very often any more.  Is this a dying technology?

hata_3396041
USB low-full-high speed peripherals
Hello It is related to this thread. https://community.cypress.com/t5/USB-Low-Full-High-Speed/CY7C65211A-Set-Line-Coding/m-p/264392#M9127 The connectio... Show More
dwaggone
USB low-full-high speed peripherals
Hello, I'm curious to know if it should be possible to send an invalid vendor request code to the Default USB device on an FX2[LP]. I know that the re... Show More
Forum Information

USB low-full-high speed peripherals

Discussion forum regarding USB low-full-high speed peripherals topics.