USB low-full-high speed peripherals Forum Discussions
Hello Infineon Support,
Thank you for your usual support.
My customer has a question.
The FTDI FT232R currently in use is in Asynchronous Bit Bang Mode.
Is there an equivalent specification for CY7C65213A?
https://www.ftdichip.com/Support/Knowledgebase/index.html?asynchronousbitbangmode.htm
Best regards,
Koki
Show LessWe are using CY7C67300 in our design to facilitate USB HOST and SLAVE functionality to our NXP controller. we are using CY7C67300 in co processor mode using hardware configuration. Now CY7C67300 obsoleted. We are planning to replace CY7C67300 with FX2/FX3.
what steps we need to follow to configure FX2/FX3 in co processor mode ?
1. Is it required to program FX2/FX3 separately to interface with our main controller?
2. Is GPIF II support parallel bus interface?
Show Less
Hi Infineon Support,
I asked a question about VCCIO in the below Community case,but there's something else I'd like to check..
In this case,It is mentioned that "VCC is used for VBUS detection where VCCIO is connected to the core and IO."
Is it correct to think that this is when power is being supplied to the VCCIO pin?
Also, if power is supplied to VCCIO but not to VCC (VBUS), what kind of control will be used?
In that case, is it correct to stop output from USBDP and USBDM?
Best regards,
Koki
Show LessAs in the title,
1. How to build the CY7C68013 development environment under WIN10?
2. I have already installed the CYUSB3014 development environment, will the two conflict?
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/%E4%BD%8E%E9%80%9F-%E5%85%A8%E9%80%9F-%E9%AB%98%E9%80%9F-USB-%E5%A4%96%E8%AE%BE/%E5%9C%A8WIN10%E4%B8%8B%E6%80%8E%E4%B9%88%E6%90%AD%E5%BB%BACY7C68013%E7%9A%84%E5%BC%80%E5%8F%91%E7%8E%AF%E5%A2%83-%E6%88%91%E5%B7%B2%E7%BB%8F%E5%AE%89%E8%A3%85%E4%BA%86CYUSB3014%E7%9A%84%E5%BC%80%E5%8F%91%E7%8E%AF%E5%A2%83-%E4%B8%A4%E8%80%85%E4%BC%9A%E4%B8%8D%E4%BC%9A%E5%86%B2%E7%AA%81/td-p/685486
Show LessHi,
I have tiny eeprom attached to FX2LP over the I2C bus.
I read about SW1 and SW2 for device to boot into Cypress FX2LP No EEPROM.
Is there additional condition such as certain bytes in certain locations of tiny eeprom to exist for this boot option to work?.
Show Less
We want to resell the CyUSB3 driver with Microsoft certificate.
Please check the information by the attached file.
If you need any other information, please let me know.
Regards,
Koji
Show Less
have anyone ever worked with this kind of microcontroller
CY7C63413C-PVXC
If already it is require to programming it or it is plug and play ?
Show LessHello
We are considering a system that uses SD2 (CYUSB2024-BZXI) to access the SD card.
【Specification】
Host side: USB2.0
SD2 side: SD (SDXC, UHS-1, SDR104 or DDR50 compatible)
Q)Is there a sample FW for SD2? Also, are there any evaluation kits equipped with SD2?
Best Regards
Show Less