Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

USB low-full-high speed peripherals Forum Discussions

USB low-full-high speed peripherals Forum Discussions

Sort by:
JuIn_1625121
USB low-full-high speed peripherals
いつもお世話になっております。 USB2.0 XCVRへのデータ転送はCPUにて実施するという認識で正しいでしょうか。 (FX3の場合は、DMAからUSB Bulk転送されるようにブロックダイアグラムに記載がありました) 以下は、FX2のブロックダイアグラムになります。 16KBもしくは、4KB の... Show More
SDR_FX3_Coder
USB low-full-high speed peripherals
Hello,  I'm trying to use FX3 as programator for FPGA. First of all, code (AN84868) for project is not available on Infineon web page: Link . Second w... Show More
TeMa_2997106
USB low-full-high speed peripherals
Is the power domain of the two pins "USBDP" and "USBDM" VCCIO? Vih and Vil are defined with reference to Vccio. Can USBDP/DM follow these specificatio... Show More
Cassie
USB low-full-high speed peripherals
Hello Community, we are Infineon colleagues and searching for a USB 2.0 to microcontroller UART converter.Because we want to use it for a customer des... Show More
rfengr84
USB low-full-high speed peripherals
Hello.  I'm using the CY7C65211 in our design as a USB to SPI bridge.  I have two questions about the operation of this device... What is the differe... Show More
man
USB low-full-high speed peripherals
Hello, We have some question on X-ray result. Why are they had different image? Are they normal? Please see attached photo.  Thanks Man Show More
TD
USB low-full-high speed peripherals
您好,关于CY7C65211的使用我还是有些疑问。我完全参考了下图的规格书设计了一块测温度的PCB,其中左侧是温度传感器,I2C方式作为从设备,CY7C65211作为主设备,右侧是USB公头接到电脑主机上,现在我手上只有一台电脑和这块PCB,可否告诉我,这么做是否有问题,CY7C65211是否只是一... Show More
CSK10
USB low-full-high speed peripherals
Hello, I am trying to commit packets using inpktend . Is there anything in particular that I need to take care of apart from FIFOADR[1:0] pins select.... Show More
CSK10
USB low-full-high speed peripherals
I have an external device which has two signals , one is start of frame and , which I use as an interrupt to the FX2lp and a data enable signal which ... Show More
TD
USB low-full-high speed peripherals
您好,我在使用CY7C65211读取传感器的I2C信号到Windows电脑上,有以下疑问盼解答。 1.使用USB-Serial Configuration Utility配置参数,显示program succed,但是使用TEST Utility时,读写测试数据,显示“write fail”和“re... Show More
Forum Information

USB low-full-high speed peripherals

Discussion forum regarding USB low-full-high speed peripherals topics.