USB low-full-high speed peripherals Forum Discussions
Hello,
I have a simple project using FX3 (CYUSB3014) and FX3 SDK 1.3.5.
I have Segger J-Link connected to the JTAG pins. Also, have a debug configuration that uses Segger J-Link GDB Server.
I see multiple errors, printed in the Console, like this:
827^error,msg="Dwarf Error: Cannot find DIE at 0x0 referenced from DIE at....
The debugger stops in main. After that, if I continue execution (Run), debugger does not respond anymore - does not stop at any breakpoint, does not allow to pause. I can only terminate the debug session.
If I change the project settings, and switch it to FX3 SDK 1.3.4 - everything works Ok.
It looks like there is something wrong with the pre-built libraries in SDK 1.3.5, as this is the only thing that really changes.
Any ideas how to get SDK 1.3.5 to work with the JTAG debugger?
Thank you,
D.
Show Less
Hi Experts,
We are using CY7C65213-32LTXIT (USB Interface IC USB-UART LP Bridge Controller) but USB detection is failed.
We are using Windows11PRO pc.
Can you share us the drivers ?
Thanks & Regards
Satrasala Raju
Show Less
Hello,
Please tell me about the pin handling of the CY7C65223-24LTXI.
When the flow control function is not used, should the RTS and CTS pins be OPEN?
Regards,
Show LessHi,
We don't understand the basics.
Please tell us about cy7c65216.
Is it possible to configure a circuit that connects multiple slave devices with different slave addresses using cy7c65216 as the master?
Is it possible to read and write any number of bytes of data from any address using the software provided by your company?
Is it correct to understand that the read and write waveforms are as shown in the figure below?
Are there any other related documents or materials other than those listed in the "More Information" section of the datasheet?
Regards,
Hi,
Under Linux system, how to
1. Confgiure CY7C65215 with programming new setting in Linux? like "USB-Serial Configuration Utility" in Windows or fwDownload.exe in command line.
2. In Linux, after re-porgramming CY7C65215 with new setting, how to enable new setting? Softare Reset or power cycle?
3. Is there document to teach customers how to use about item 1 and 2?
Regards,
Kyle
Show Less
Hello, please tell me a question. If we connect multiple CYUSB3014 devices to the PC and open them at the same time, how can we set the bulkEndpoint for each device at this time, because from the existing routine, I see that bulkEndpoints are all obtained through ccyUSBDevice, and ccyUSBDevice is only instantiated once
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/%E4%BD%8E%E9%80%9F-%E5%85%A8%E9%80%9F-%E9%AB%98%E9%80%9F-USB-%E5%A4%96%E8%AE%BE/PC%E6%9C%BA%E4%BD%BF%E7%94%A8%E5%A4%9A%E4%B8%AACYUSB3014%E8%AE%BE%E5%A4%87-%E5%90%8C%E6%97%B6%E6%89%93%E5%BC%80%E5%A6%82%E4%BD%95%E5%AF%B9%E6%AF%8F%E4%B8%AA%E8%AE%BE%E5%A4%87%E8%AE%BE%E7%BD%AEBulkEndPoint%E5%91%A2/td-p/679775
Show Lesshi,
i have wrote a simple to code to access the esp8266 via I2C.
bilnk led and i2c_write ; LOOP
when the SDL is not connected to the ESP8266,the loop repeats (led blinks and I can see the SCL and SDA in logic analyzer).
the moment i connect the SDL line to the ESP8266, the code hung up.
Note ;
1. The connections are correct .
2. The FX2 kit has pull up (2.2K)resistors on both SCL and SDA line.
3. SDCC compiler is used.
Please suggest ways to resolve or debug.
Thank you.
Show Less