USB low-full-high speed peripherals Forum Discussions
I have access to the below site.
https://www.infineon.com/cms/en/design-support/software/code-examples/usb-controllers-code-examples/...
in the Code Examples integrated with Application Notes. I try to find the example code for AN63787. But it has no link to download. Can anyone suggest to me how I can find the link?
Show LessHello,
CY7C68013A-56BAXC's datasheet P26 , Table 11.
XTALIN
"It is also correct to drive XTALIN with an external 24-MHz square wave derived from another clock source. When driving from an external source, the driving signal should be a 3.3-V square wave."
What are the details of the input clock specifications? Ex. Accuracy
Regards,
Show LessGood day,
I am here because i am in desperate need for help. I am a neurophysiologist in a low income country who just got an old EMG machine for use on our patients as the older machine is bad
Tried connecting the machine to the computer (Win XP, Win 7, Win 10) but it seems the OS is not recognizing the device for which i suspect a driver issue. I can see a Cypress EZ-USB, FX, FX2, and SX2 Development Kit 2.30.710 installed when i install the software that come with the machine.
I am looking for assistance on how to get the computer to recognize the machine as i feel its something with the driver setting
If this is not the right medium, can i please to connected with someone who can help?
Below is a picture of the error i get when i try to use the machine
Show Less
Hello Everyone !
I have attached Flash Nands with my Controller and am using it as a usb(MSC) drive.
How to read/write file or data to a certain address to the nand and verify it by a fixed command over uart before enumerating as msd.
Basically the purpose here is to verify health of the attached nands
Any help would be highly appreciated.
Regards,
Show Less
I have access to the below site.
in the Code Examples integrated with Application Notes. I try to find the example code for AN61345. But it has no link to download. Can anyone suggest to me how I can find the link?
Show LessThe obsolete PLX Net2272 USB 2.0 Peripheral Controller is used our existing design. It is an interfaces between a parallel 8 bit bus and USB. This part does not require software to be loaded in order to work. I found the closest Infineon match to be the CY7C68013A, but it requires programming. Does Infineon have an 8 bit parallel bus to USB 2.0 that does not require programming?
Show LessHi,
We are using CYUSBS234 to expand GPIOs via USB. We are using IMX8MM board for the development.
Please provide information about the device driver and device tree integration in yocto for CYUSBS234.
How these GPIOs can be assigned?
SOM: IMX8MM
BSP: Yocto Zeus
Regards,
Bhargava
Show LessHi All,
I have fx2lp device, when usb plug in Industrial PC and turn on IPC.
the problem will appear as below after IPC is turned on
it is install Windows Embedded Standard 7 SP1 in IPC.
Have any suggestion about this issue?
BR,
Darren
Show LessHi,
Need your help here.
Right now my application is using End Point 2 with 512bytes as the buffer size for bulk transfer.
Once Cypress chip receives 512Bytes, bit 1 (EP2EF) of EP24FIFOFLGS is set to zero.
How to configure EndPoint2 to receive less than 512bytes and which register to poll for when EP2 is configured to receive less than 512Bytes.
Show Less