Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

USB low-full-high speed peripherals Forum Discussions

USB low-full-high speed peripherals Forum Discussions

Sort by:
yazan_ee
USB low-full-high speed peripherals
Hi, Can anyone help me with installation of cyusb suit for linux. I followed the step given in the readm-me file, but end up with no output. I attache... Show More
Yosuf
USB low-full-high speed peripherals
We have a product using a CY7C68013 FX2LP processor connected to a host via High Speed USB.  Currently the host is a tablet with an X86 processor runn... Show More
Justy
USB low-full-high speed peripherals
Hi, Could you provide Linux sample codes for getting and setting GPIO config from and to CY7C65215 ? Because there are only  sample codes of getting a... Show More
kk2022
USB low-full-high speed peripherals

CY7C65210不知道如何无法配置gpio,在windows下的设备管理器上看到设备是Billboard Interface。驱动也有下载了,正常应该是Cypress USB-Serial Configuration Utility上面可以配置的GPIO的功能

CSK10
USB low-full-high speed peripherals
Hello, I have an application which should monitor  two ready pins and then trigger the data transaction. However, when I check the GPIFREADYSTAT regis... Show More
CSK10
USB low-full-high speed peripherals
Hello,   Can someone provide me a link to the firmware  for the AN66806  application note. I couldn't find it attached.   Thanks Show More
Justy
USB low-full-high speed peripherals
Hi,  We are validating RTS/CTS flow control of UART vendor mode on CYUSB236 EVK by sending a 7MB text file from SCB0 to SCB1. With referring to Cypres... Show More
yazan
USB low-full-high speed peripherals
  Hi, On the FX2LP, I'm performing a 16-bit single read/write operation. Using the Control Center's Transfer IN button, I read 512 bytes in a single a... Show More
geashill
USB low-full-high speed peripherals
i have cypress hub usb manufacturing driver in dell aurora r4, x 64 based, windows 10 service tag 5W56422. the driver is version  1.2.3.14     driver ... Show More
YoungZhang
USB low-full-high speed peripherals
Do CY7C65211-24LTXI has a Linux driver?  Can it be supported in Linux(Ubuntu)? I only can found Windows driver for it. Chinese describe/中文描述: 这款芯片有lin... Show More
Forum Information

USB low-full-high speed peripherals

Discussion forum regarding USB low-full-high speed peripherals topics.