Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

USB low-full-high speed peripherals Forum Discussions

CSK10
USB low-full-high speed peripherals

Hello,

Is there a possibility to store data stream coming into the Host in some text format or any other format ? 

SDR_FX3_Coder
USB low-full-high speed peripherals
Hello,  I'm trying to use FX3 as programator for FPGA. First of all, code (AN84868) for project is not available on Infineon web page: Link . Second w... Show More
TeMa_2997106
USB low-full-high speed peripherals
Is the power domain of the two pins "USBDP" and "USBDM" VCCIO? Vih and Vil are defined with reference to Vccio. Can USBDP/DM follow these specificatio... Show More
Cassie
USB low-full-high speed peripherals
Hello Community, we are Infineon colleagues and searching for a USB 2.0 to microcontroller UART converter.Because we want to use it for a customer des... Show More
man
USB low-full-high speed peripherals
Hello, We have some question on X-ray result. Why are they had different image? Are they normal? Please see attached photo.  Thanks Man Show More
CSK10
USB low-full-high speed peripherals
Hello, I am trying to commit packets using inpktend . Is there anything in particular that I need to take care of apart from FIFOADR[1:0] pins select.... Show More
GrCa_1363456
USB low-full-high speed peripherals
Can additional SPI_Select, chip select lines, be added to a Serial Communication Bus (SCB) interface of CY7C65215/A when in SPI Master mode? Greg Show More
NXTY_Nishinaga
USB low-full-high speed peripherals
Hello, I would like to change the VID/PID from the default value to a custom value. Referring to chapter 3.1 of the Cypress USB-Serial Configuration U... Show More
GrCa_1363456
USB low-full-high speed peripherals
Please clarify if Ordering part number CY7C65215A-24LTXI is a typo or if Infineon plans to offer a CY7C65215A in a 24 pin package. Page 1 of Data shee... Show More
Jack-be-nimble
USB low-full-high speed peripherals
I'm trying to upload a custom configuration to the CY7C65215A using the terminal based configuration utility in Linux Ive generator an encrypted.cyusb... Show More
Forum Information

USB low-full-high speed peripherals

Discussion forum regarding USB low-full-high speed peripherals topics.