USB low-full-high speed peripherals Forum Discussions
HI,
I am currently working on a project to get the video out of a camera using a FX2LP. I am trying to understand the FIFO read using GPIF. I have attached the FSYNC to RDY0 and LSYNC to RDY1. The hardware seems to work right as i able to receive the data out of the camera using a single read byte. I want to FIFO read waveform so that i can get the SYNC frame out of the camera and get the video out of the camera. But i still don't understand completely the transition from the timing diagrams to the state diagrams using GPIF. The following points, I am having confusion with:
1. In my project, FSYNC will rise at least one clock cycle before LSYNC. I want to make sure that FSYNC and LSYNC are both 0 before i activate the data. But if the decision state I can't use if FYSNC = 0 and LSYNC = 0 because the second data value is always 1.
2. What should i use for the transaction counter? i am receiving 1 byte per pixel and it is 320 x 240 camera. Should i use the transaction counter to be 76800? I am confused that should I get frame in each FIFO read transaction. If yes, i want to use the AUTO IN mode, will the data be transferred automatically once the data buffer filled with 512 bytes?
I am attaching the timing diagram of the camera. Can you suggest any what would be the best way for me to get the video out of the camera.
I would really appreciate if someone can help me with this issue.
Regards,
ABM
Show LessHi
I'm debugging a Bulkloop project with mon-int-sio0.
When I trace to EZUSB_Discon(TRUE), the device renumerates as an unknown device.
Can somebody give me some suggestion on this?
Thanks.
Show LessHi,
I am using FX2LP developement kit. I am stuck when i try to external clock i can't do Bulk In Transfer. This is my project is:
I am trying to connect FX2LP with an external device (camera). The problem is that I want to use the clock of camera which is running at 5 MHZ so that i can synchronize my LSYNC(HSYNC) AND FSYNC(VSYNC) and grab a frame out of the camera. I implemented GPIF single read just to make sure that i able to receive any data from the camera. I used the GPIF example to data from the camera. Program runs fine and give me data if i use internal clock. But when i use external clock, my bulk in transfer fails in CyConsole. Could you please help me. That would be really appreciated.
Regards,
ABM
Show LessHi,
I'm trying to understand exactly what happens when the FX2 has power but the USB is unplugged and then re-plugged back in. Our firmware uses the vend_ax example as skeleton code. I had thought originally that if the user unplugs the USB cable and plugs it back in (power is supplied separately; not through USB) that TD_Init() would be called again. However, that appears to not be the case. I understand that when the USB is unplugged the FX2 will go into sleep mode and that it "wakes up" when the USB cable to the host is plugged back in.
My issue is, given how our FX2 and FPGA are integrated, I need to send a signal from the microcontroller to reset the FPGA when this re-enumeration event happens and I'm not sure what routine will be called once when the USB cable is inserted. I found somewhere that TD_Init() is called when "re-enumerating a new device" but apparently unplugging and plugging in USB cable connecting to the host is not that event?
Any wisdom welcome!
-Hyped
Show LessHi
I want find ack signal in EZUSB_i2c function.
But i have not oscilloscope so i need to find way without oscilloscope to find ack status .
And i want find status ack signal in read or write in i2c.
So, is there any way how to find ack signal ?
Show LessCypress’s PRoC™-UI Solution Wins 2012 Product of the Year Award From Electronic Products Magazine
Please refer to the following webpage for more details on PRoC-UI
http://www.cypress.com/?id=4598
Thanks,
Sai Krishna.
Show LessGreetings.
We make a line of data collection hardware that connects to Windows/Mac/Linux machines via USB.
Our latest product uses the CY8C5247AXI PSoC5 processor as our controller.
Up until now, it has worked fine with all host computers that we have connected to (Mac OSX and Windows XP & 7).
When we connect our device to a Dell Latitude 10 tablet running Windows 8, the USB connection works fine most of the time, but occasionally we see on our USB protocol analyzer that some IN transactions from the host are ignored by the PSoC. I'm guessing there is some sort of subtle signalling issue that is causing the failures.
Attached is an image showing what our protocol analyzer sees.
Any ideas on how to fix this problem would be greatly appreciated.
Thank you
Scott Wild
Pasco scientific
Show Lesshi im using the fx2 on windows 8 and the first enumeration works but the second doesnt. This worked on windows 7 but when i move to windows 8 something goes wrong. What could be the possible issue ?
Thankyou 🙂
Show Less