Hi ,
Please provide the MTBF/FIT value for the following:
#1. CY7C64215-56LTXC
Thank you,
Hi,
We use CY7C68013 in a data capture card, CY7C68013 connect to a FPGA. When we use FPGA send a RESET# (active low about 5ms)signal, sometimes the software transfer failed. And we use USBTrace, Dectect SURPRISE REMOVAL. how can we fix it? Thank you!
The USBTrace detect as below.
Show Less
Hello,
We are using the CY7C65211 bridge on a device that connect to a Linux (Kubutu 18.04) machine. The Linux PC, instead of adding a serial port (/dev/ttyXXX) is listing the device as a Thermometer:
Bus 001 Device 057: ID 04b4:0002 Cypress Semiconductor Corp. CY7C63x0x Thermometer
I downloaded CP210x_SDK from the website and install it, but the serial port appears nowhere.
In a Windows PC, the serial port works out-of-the-box, but I can't seem to make it work in Linux (no /dev/ttyUSBx or /dev/ttyACMx, or anything).
What am I missing?
Thank you so much!
Héctor
Show LessHello Everyone !
I have attached Flash Nands with my Controller and am using it as a usb(MSC) drive. Is it possible to use uart protocol after enumeration has been done.
For example after having a certain file written or any file written to the flashes can we send a command or signal over the UART0 or UART1.
If yes then how?
If no then why?
Any help in this regard would highly be appreciated.
Regards,
Show LessI have access to the below site.
https://www.infineon.com/cms/en/design-support/software/code-examples/usb-controllers-code-examples/...
in the Code Examples integrated with Application Notes. I try to find the example code for AN63787. But it has no link to download. Can anyone suggest to me how I can find the link?
Show LessHello,
CY7C68013A-56BAXC's datasheet P26 , Table 11.
XTALIN
"It is also correct to drive XTALIN with an external 24-MHz square wave derived from another clock source. When driving from an external source, the driving signal should be a 3.3-V square wave."
What are the details of the input clock specifications? Ex. Accuracy
Regards,
Show LessGood day,
I am here because i am in desperate need for help. I am a neurophysiologist in a low income country who just got an old EMG machine for use on our patients as the older machine is bad
Tried connecting the machine to the computer (Win XP, Win 7, Win 10) but it seems the OS is not recognizing the device for which i suspect a driver issue. I can see a Cypress EZ-USB, FX, FX2, and SX2 Development Kit 2.30.710 installed when i install the software that come with the machine.
I am looking for assistance on how to get the computer to recognize the machine as i feel its something with the driver setting
If this is not the right medium, can i please to connected with someone who can help?
Below is a picture of the error i get when i try to use the machine
Show Less
Hello Everyone !
I have attached Flash Nands with my Controller and am using it as a usb(MSC) drive.
How to read/write file or data to a certain address to the nand and verify it by a fixed command over uart before enumerating as msd.
Basically the purpose here is to verify health of the attached nands
Any help would be highly appreciated.
Regards,
Show Less
I have access to the below site.
in the Code Examples integrated with Application Notes. I try to find the example code for AN61345. But it has no link to download. Can anyone suggest to me how I can find the link?
Show LessThe obsolete PLX Net2272 USB 2.0 Peripheral Controller is used our existing design. It is an interfaces between a parallel 8 bit bus and USB. This part does not require software to be loaded in order to work. I found the closest Infineon match to be the CY7C68013A, but it requires programming. Does Infineon have an 8 bit parallel bus to USB 2.0 that does not require programming?
Show Less