USB low-full-high speed peripherals Forum Discussions
With a CY7C65211 board and the example from the USB-Serial SDK spimaster, I am able to transfert 32k of data
from SPI EEPROM 25AA256 to the computer. But I only get 12Kbyte/s.
Should I get more at 3 Mhz ?
See attached code
Show LessHi,
I am beginning to use a CY7C68013A , It's connected to a FPGA Altera Cyclone (I), I've connected the USB Chip to the computer and I've modified the cyusb.inf file using the VID=04B4 and PID=8613 (default), in the device manager it's seems OK, but i have noticed that when i change VID or PID to a different value still in the device manager it's OK,.
I've used "USB Control Center" to send some bytes to the USB Chip (default firmware) but it doesn't work , it gives the message :
BULK OUT transfer
BULK OUT transfer failed with Error Code:997
Should it work?or i need to program a different firmware??
Then i have tried with the example "Designing with EZ-USB FX2LP Slave FIFO Interface using FPGA " (just used slave.hex)
and the Device manager shows the VID= 04B4 and PID=00F1, I've modified the "cyusb.inf" file usind the new VID and PID, but the Device manager of my windows 7 shows :
The drivers for this device are not installed. (Code 28)
The install class is not present or is invalid.
To find a driver for this device, click Update Driver.
So, i've tried update the driver using the driver from C:\Cypress\Cypress Suite USB 3.4.7\Driver\bin\wlh\x64 (It's same path of cyusb.inf)
"The install class is not present or is invalid" (look in DevManager.png)
I hope someone can help me.
thanks in advance
Show Lessquestion1:
What version of the software development environment does 63743 use? where to downoad?
question2:
What simulator to programme 63743? like 68013?
question3:
which chip can perfectly replace 63743, our project is about keyboard mouse, so need USB and PS / 2 port?
thanks.
Show LessHi,
I am working with FX2LP. I have found examples relating to bulk and isochronous transfer, but not with interrupt transfer. Are there any examples with interrupt transfer, for windows side and FX2LP side?
Thanks,
Begos
Show LessWhere can I see examples of CyUSB.dll call functions when programming in Visual Basic.NET?
Such examples are there?
The document "Cypress CyUSB .NET DLL Programmer's Reference" there are only examples for Visual C #
Thanks.
I am a new learner!Could Anyone give me the FX2LP Slave FIFO firmware?
We are supplied by cypress with usb drivers ( inf, cat, sys). The desktop application I support is written with java so we use a install4j to create an app installer and we use a bat file to start dpinsta.exe to do the driver install.
I need some guidance on what is a better way to do this today? I was poking around at Microsoft and the new windows 10 wdk. I also noticed that cypress now provides a WdfCoinstaller01011.dll. How do we use this? How can i create a driver install package?
Thank you
Show LessHello!
The aplication note proposes to react to a flag within a single cycle.
When I take the Clock to FLAGS output propagation delay of 9.5/13.5 ns how am I supposed to react to it within one period of 20.83 ns without violating the 18.7/12.7 ns setup time of SLRD or 10.4/12.1 ns of SLWR? As this is clearly not possible and I have not found a single implementation caring, what would be the correct way to implement it?
Also I couldn't find any information weather it is legal to assert SLRD while the FIFO is empty or SLWR while full. Can anyone point me to that information?
best regards
Markus
If I have an instance of a CyUSBDevice from the .NET DLL, is there any way to pass this to a native DLL as a CCyUSBDevice?
I.e. can I convert a CyUSBDevice to a CCyUSBDevice?
Show Lessi download the hex into fx2lp's ram ,but it can not function , so i use the oscillograph to view the waveform of SDA pin.it shows that ,as long as i download the hex file into the ram using the control panel and click the reconnect button , the waveform is a endless square wave . after that, my control panel crashed. what should i do ???
Show Less