USB low-full-high speed peripherals Forum Discussions
text.format{('custom.tabs.no.results')}
Hello,
I have implemented successfully cdc class in fx2lp firmware,i can recieve data from the fx2lp to pc(usb serial).
how can i check baudrate in this situation like in normal uart baud rate (baudrate settings require on both tx and rx side)?
how it will be configured in fx2lp side(firmware)?
in windows side,we are setting 9600bps in hercules terminal?
regards,
geetha.
Show LessI can't install CYUSB236 DVK software in my PC.
When I try to install, CyInstaller is said , "Microsoft VC ++ 2008 Redistributable is not install".
However, various versions of Redistributable package (including Ver. 2008) have already installed on the PC.
Why can't I install?
Is there anything else I should do?
Show Less
Hello, Cypress expert,
I have a question about the EZ-USB FX2. I am using uVision Toolchain C51 compiler/Assembler Kit Version:9.56.0.0.
after compile, it generates a hex file. I run "HEX2BIX -IR -M 16384 -F 0xC2 -O Scan_BD_FW.iic Scan_BD_FW.hex" to convert it to iic format,
this iic file works fine with cyconsole. but if I use the hex file write to microchip 24lc128. the system not work.
so I have to use Cyconsole to load the iic file to this eeprom. and use the eeprom programmer to read the master chip file out. then load this file to the chip.
I don't understand why the Hex file can't be used directly to load the EEprom. is there any trick? do we need to setup some special parameter of the eeprom programmer to make it work.
Thanks,
David Sun
Show Lesshello ,
we are using the CDC Class in FX2LP to write data to port we want to set the baud rate more than 921600 when i referred the application note AN58764 maximum baud rate is 115200 . how to increase that baud rate to around 921600 . if any one has idea please let me know .
thanks regards,
veerendra
Show LessHi,
I'm using CY7C68013A-56BAXC and I have a problem about heating issue of this device.
Heating occured after device configured.
What makes this device heating?
I think some register of device makes heating.
Please advice me about this heating issue.
Best Regards,
Matthew
Show LessGood afternoon all,
Am trying to blink an led using fx2lp breakout board. We connected one led at pin portA.0. By keeping examples program as reference given in the fx2lp dvk kit website We written the code for this one. We are getting error as shown below.
Please let me know how to solve this problem.
#include<reg51F.h>
sbit led = PA.0;
void wait(int x)
{
int i, j;
for(i = 0; i<x; i++)
{
for(j = 0; j<25; j++);
}
}
int main()
{
while(1)
{
led = 1;
wait(100);
led = 0;
wait(100);
}
return 0;
}
Regards
Vimala
Hi ,
We are using cypress USB products .when we will connect to PC via USB and checked in Device manager these devices comes under Universal serial Bus controller category but we want as imaging Device because we interfaced with image sensor i have attached the screenshot PFA. So we wanted to change from Universal serial Bus controller category to imaging Device .Can any one help me to change ?.
Thanks Regards ,
Veerendra
Show LessHi Cypress,
for production, we need to program the EEPROM 24LC128 for Cy7c68013, it is easier to program the chip with a standalone programmer. but the programmer only loads HEX file.
the HEX file compiled from uvision can't be used for this purpose.
what we can do is use HEX file, convert to iic format, then load to 24lc128 on a developing board. then use the programmer to copy the image to a file. then burn this file to the EEPROM. is there a way to generate a HEX file can be burned in the EEPROM directly.
Thanks,
David Sun
Show LessI have an application to transmit 640x480 image sesnor data over FX2LP USB 2.0 using UVC through FPGA. I tried to find the firmware online, but no result. Then I tried to develop it myself, but it did not work .Can any one provide it ,thanks
Show LessHello!
I want to implement UVC using FX3 (trying on SuperSpeed Kit). There is no problem with UVC examples from SDK, but I have no luck to modify USBVideoClass example to work with uncompressed frames. I've downloaded specs from USB.org - USB Device Class Specifications and changed format and frame descriptors as described. I've also changed Probe and Commit control structs.
Is there any example of FRAME_UNCOMPRESSED video translation?
v4l2-ctl output:
v4l2-ctl --all -d0
Driver Info (not using libv4l2):
Driver name : uvcvideo
Card type : FX3
Bus info : usb-0000:00:14.0-5
Driver version: 4.15.18
Capabilities : 0x84200001
Video Capture
Streaming
Extended Pix Format
Device Capabilities
Device Caps : 0x04200001
Video Capture
Streaming
Extended Pix Format
Priority: 2
Video input : 0 (Camera 1: ok)
Format Video Capture:
Width/Height : 32/24
Pixel Format : 'BGR3'
Field : None
Bytes per Line : 96
Size Image : 2304
Colorspace : Default
Transfer Function : Default (maps to Rec. 709)
YCbCr/HSV Encoding: Default (maps to ITU-R 601)
Quantization : Default (maps to Full Range)
Flags :
Crop Capability Video Capture:
Bounds : Left 0, Top 0, Width 32, Height 24
Default : Left 0, Top 0, Width 32, Height 24
Pixel Aspect: 1/1
Selection: crop_default, Left 0, Top 0, Width 32, Height 24
Selection: crop_bounds, Left 0, Top 0, Width 32, Height 24
Streaming Parameters Video Capture:
Capabilities : timeperframe
Frames per second: 25.000 (25/1)
Read buffers : 0
I'm using guvcview utility to check results. And here is the log:
...
V4L2_CORE: (get_v4l2_frame) video stream must be started first
V4L2_CORE: (get_v4l2_frame) video stream must be started first
V4L2_CORE: (get_v4l2_frame) video stream must be started first
V4L2_CORE: (get_v4l2_frame) video stream must be started first
...
lsusb output:
Show Less
Bus 001 Device 047: ID 04b4:4722 Cypress Semiconductor Corp.
Device Descriptor:
bLength 18
bDescriptorType 1
bcdUSB 2.10
bDeviceClass 239 Miscellaneous Device
bDeviceSubClass 2 ?
bDeviceProtocol 1 Interface Association
bMaxPacketSize0 64
idVendor 0x04b4 Cypress Semiconductor Corp.
idProduct 0x4722
bcdDevice 0.00
iManufacturer 1 Cypress
iProduct 2 FX3
iSerial 0
bNumConfigurations 1
Configuration Descriptor:
bLength 9
bDescriptorType 2
wTotalLength 198
bNumInterfaces 2
bConfigurationValue 1
iConfiguration 0
bmAttributes 0x80
(Bus Powered)
MaxPower 400mA
Interface Association:
bLength 8
bDescriptorType 11
bFirstInterface 0
bInterfaceCount 2
bFunctionClass 14 Video
bFunctionSubClass 3 Video Interface Collection
bFunctionProtocol 0
iFunction 0
Interface Descriptor:
bLength 9
bDescriptorType 4
bInterfaceNumber 0
bAlternateSetting 0
bNumEndpoints 1
bInterfaceClass 14 Video
bInterfaceSubClass 1 Video Control
bInterfaceProtocol 0
iInterface 0
VideoControl Interface Descriptor:
bLength 13
bDescriptorType 36
bDescriptorSubtype 1 (HEADER)
bcdUVC 1.00
wTotalLength 80
dwClockFrequency 48.000000MHz
bInCollection 1
baInterfaceNr( 0) 1
VideoControl Interface Descriptor:
bLength 18
bDescriptorType 36
bDescriptorSubtype 2 (INPUT_TERMINAL)
bTerminalID 1
wTerminalType 0x0201 Camera Sensor
bAssocTerminal 0
iTerminal 0
wObjectiveFocalLengthMin 0
wObjectiveFocalLengthMax 0
wOcularFocalLength 0
bControlSize 3
bmControls 0x00000000
VideoControl Interface Descriptor:
bLength 12
bDescriptorType 36
bDescriptorSubtype 5 (PROCESSING_UNIT)
Warning: Descriptor too short
bUnitID 2
bSourceID 1
wMaxMultiplier 16384
bControlSize 3
bmControls 0x00000000
iProcessing 0
bmVideoStandards 0x1c
PAL - 625/50
SECAM - 625/50
NTSC - 625/50
VideoControl Interface Descriptor:
bLength 28
bDescriptorType 36
bDescriptorSubtype 6 (EXTENSION_UNIT)
bUnitID 3
guidExtensionCode {ffffffff-ffff-ffff-ffff-ffffffffffff}
bNumControl 0
bNrPins 1
baSourceID( 0) 2
bControlSize 3
bmControls( 0) 0x00
bmControls( 1) 0x00
bmControls( 2) 0x00
iExtension 0
VideoControl Interface Descriptor:
bLength 9
bDescriptorType 36
bDescriptorSubtype 3 (OUTPUT_TERMINAL)
bTerminalID 4
wTerminalType 0x0101 USB Streaming
bAssocTerminal 0
bSourceID 3
iTerminal 0
Endpoint Descriptor:
bLength 7
bDescriptorType 5
bEndpointAddress 0x82 EP 2 IN
bmAttributes 3
Transfer Type Interrupt
Synch Type None
Usage Type Data
wMaxPacketSize 0x0040 1x 64 bytes
bInterval 8
Interface Descriptor:
bLength 9
bDescriptorType 4
bInterfaceNumber 1
bAlternateSetting 0
bNumEndpoints 0
bInterfaceClass 14 Video
bInterfaceSubClass 2 Video Streaming
bInterfaceProtocol 0
iInterface 0
VideoStreaming Interface Descriptor:
bLength 14
bDescriptorType 36
bDescriptorSubtype 1 (INPUT_HEADER)
bNumFormats 1
wTotalLength 71
bEndPointAddress 131
bmInfo 0
bTerminalLink 4
bStillCaptureMethod 1
bTriggerSupport 1
bTriggerUsage 0
bControlSize 1
bmaControls( 0) 27
VideoStreaming Interface Descriptor:
bLength 27
bDescriptorType 36
bDescriptorSubtype 4 (FORMAT_UNCOMPRESSED)
bFormatIndex 1
bNumFrameDescriptors 1
guidFormat {7deb36e4-4f52-ce11-9f53-0020af0ba770}
bBitsPerPixel 24
bDefaultFrameIndex 1
bAspectRatioX 0
bAspectRatioY 0
bmInterlaceFlags 0x00
Interlaced stream or variable: No
Fields per frame: 2 fields
Field 1 first: No
Field pattern: Field 1 only
bCopyProtect 0
VideoStreaming Interface Descriptor:
bLength 30
bDescriptorType 36
bDescriptorSubtype 5 (FRAME_UNCOMPRESSED)
bFrameIndex 1
bmCapabilities 0x00
Still image unsupported
wWidth 32
wHeight 24
dwMinBitRate 460800
dwMaxBitRate 921600
dwMaxVideoFrameBufferSize 2304
dwDefaultFrameInterval 400000
bFrameIntervalType 1
dwFrameInterval( 0) 400000
Binary Object Store Descriptor:
bLength 5
bDescriptorType 15
wTotalLength 22
bNumDeviceCaps 2
USB 2.0 Extension Device Capability:
bLength 7
bDescriptorType 16
bDevCapabilityType 2
bmAttributes 0x00000002
Link Power Management (LPM) Supported
SuperSpeed USB Device Capability:
bLength 10
bDescriptorType 16
bDevCapabilityType 3
bmAttributes 0x00
wSpeedsSupported 0x000e
Device can operate at Full Speed (12Mbps)
Device can operate at High Speed (480Mbps)
Device can operate at SuperSpeed (5Gbps)
bFunctionalitySupport 3
Lowest fully-functional device speed is SuperSpeed (5Gbps)
bU1DevExitLat 0 micro seconds
bU2DevExitLat 0 micro seconds
Device Status: 0x0000
(Bus Powered)