Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

USB low-full-high speed peripherals Forum Discussions

fenghongchen
Level 1
Level 1
First question asked Welcome!

我arm开发板采用的是rk3568,在开发板中fx3是可以正常工作的,但我把程序交叉编译到arm中后,将rk3568单独放置在另一个底板中,然后连接fx3,fx3是可以被识别的,打开也可以,但没有数据。系统是ubuntu18.04,arm板中也是对应的arm板系统(GNU/Linux 4.19.206 aarch64),usb通信采用的libusb编写的,也是交叉编译。在pc端的系统中fx3正常工作,在firefly开发板中配合rk3568也是可以正常工作,但当rk3568替换到其他底板的时候就出问题了,会报错“can't set config #1,error -110”。同样的硬件环境下,我把fx3用其它类似功能的芯片替代是没有问题的,都可以正常工作,只有fx3是不可以正常工作,我不确定在arm中我需要什么配置吗?我看在linux的sdk中看到那个cyulibusb应该也是用libusb包装的,我理解不需要特殊编译就可以,因为我一直使用的是libusb

0 Likes
1 Reply
JiangJing
Moderator
Moderator
Moderator
First question asked 100 sign-ins 25 solutions authored

Hi,

       想了解一下,你是在ARM下都无法正常工作吗?看您的描述中似乎FX3+rk3568 arm开发板是可以正常工作,您是在其中一个底板中ARM是可以正常工作的,但是换一个底板,相同的软件FX3不能正常工作?

0 Likes
This widget could not be displayed.