- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
I have an application based on the Vend_ax sample. I have one command that will not send a response back. I load EP0, but it is never sent.
If I comment out #1 and #2, then I get a response back, but I do not get my two bytes of data after the control "header".
case VR_XSVF_COMMAND:
#if 1 //jad ENABLE_FPGA_PROGRAMMING
EP0BCH = 0; //<<<<<#1
EP0BCL = 0; // Clear bytecount to allow new data in; also stops NAKing //<<<<<#2
while(EP0CS & bmEPBUSY);
blockLen = EP0BCL;
for(i=0; i<blockLen; i++)
{
fileStorage = *(EP0BUF+i);
}
#if 0 //jad
if (xsvfFirstCommand == 1)
{
xsvfFirstCommand = 0;
xsvfInitialize();
}
*EP0BUF = xsvfRun();
#endif
//jad*EP0BUF = 0xFF;
#else
*EP0BUF = 0xFF;
#endif // ENABLE_FPGA_PROGRAMMING
EP0BCH = 0;
EP0BCL = 1; // Arm endpoint with # bytes to transfer
EP0CS |= bmHSNAK; // Acknowledge handshake phase of device request
break;
The PC code is (cmd[] = 0x07 0x00) :
if
(myDev != null)
{
//jad implement sending to board
{
myDev.ControlEndPt.ReqType =
myDev.ControlEndPt.Direction =
myDev.ControlEndPt.ReqCode = (
myDev.ControlEndPt.Value = (
myDev.ControlEndPt.Index = (
if (myDev.ControlEndPt != null ) CyConst .REQ_VENDOR; CyConst .DIR_FROM_DEVICE; byte ) Commands .VR_XSVF_COMMAND; ushort )cmd.Length; ushort )0; int len = cmd.Length; if (myDev.ControlEndPt.XferData( ref cmd, ref len)) return ( XSVFErrorCodes )cmd[0]; else
}
}
return XSVFErrorCodes .XSVF_USB_COMMAND_FAILED; return XSVFErrorCodes .XSVF_NO_DEVICE;
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi dreitz,
This is expected as you are assigning the EP0BCL register at the begining of the vendor command ,
EP0BCH = 0; //<<<<<#1
EP0BCL = 0; // Clear bytecount to allow new data in; also stops NAKing //<<<<<#2
This will commit the EP0 buffer with 0 bytes and you would not receive any data.You should first initialize the buffer and then write to these registers as you are doing at the end in your code.
-shub