Announcements

Learn how to optimise USB-C for your designs at 18 May's USB-C PD Webinar.
Click here to register.

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Anonymous
Not applicable

Dear sir,

   

i ahve developed one code to download my firmware to cypress FX2LP. i am using the  cyusb's cyusb_control_transfer and i am catching the sent bytes and i get perfect match between the Bytes sent and the firmware file size

   

but sad part is my device doesnt get initialised

   

Note: Firmware is tested n works fine

   

i am pasting here my code please do rply and give suggestions.

   

 

   

#include <stdio.h>
#include <stdlib.h>
#include <time.h>
#include <string.h>
#include <unistd.h>
#include <sys/stat.h>
#include <fcntl.h>
#include "../../include/cyusb.h"



unsigned int DownloadFirmware();


int main (void)
{

unsigned int a = 0;

a = DownloadFirmware();

if(a == 1)
{
printf("\nsuccessful fd\n");
}

}


unsigned int DownloadFirmware()
{

        cyusb_handle *h;
        int size, r;
        int a, b, c, flag;
    int Sum = 0, Done = 0;
    const char *cbuf;
    const char *filename = "/home/usb/FPR/firmware/fw.bix";
    unsigned char *buf = NULL;
    unsigned char *ptr;
    unsigned char num_bytes = 0;
    unsigned short address = 0;
    unsigned char reset = 0;
    FILE *fp;   /* file pointer */
   



        struct libusb_device_descriptor desc;


        a = cyusb_open();

         if ( a < 0 ) {
              printf("Error opening library\n");
              return -1;
           }
        else if ( a == 0 ) {
                   printf("No device foundd\n");
           }

        h = cyusb_gethandle(0);
        b = cyusb_get_device_descriptor(h, &desc);

        if(b){
           printf("error getting device descriptor\n");
           return -2;
        }




        struct stat st;
        stat(filename, &st);
        size = st.st_size;
       
        printf("size of file = %d\n", size);   
   
            buf = (unsigned char*)malloc(size);       




     /* open file for read */
          if ((fp = fopen("/home/usb/FPR/firmware/fw.bix", "r"))==NULL){
              printf("Cannot open file \n");
        }     

        fread(buf, size, 1 ,fp);
   
        fclose(fp);
    if(buf)
    printf("file copied");

    int ChunkSize = 4000; // seem to sending 4000 but not 5000 at one time
    int BlockSize = size;
    int entry = 0;
    reset = 1;
    sleep(1);


    reset = 0;

        r = cyusb_control_transfer(h, 0x40, 0xA0, 0xE600, 0x00, &reset, 0x01, 1000);
        if (!r) {
           printf("Error in control_transfer\n");
           return r;
        }

    sleep(1);
    sleep(1);
   
    ptr = buf;
   
    while(!Done)
    {


            if(BlockSize < ChunkSize){
                                address += ChunkSize;
                   //             buf = buf+ChunkSize;
                             ptr = ptr + ChunkSize;
                                ChunkSize = BlockSize;
                                flag = 1;
                                }


     r = cyusb_control_transfer(h, 0x40, 0xA0, address, 0x00, ptr, ChunkSize, 30);

        printf("\nturn no. %d\n", r);
         if (!r) {
               printf("Error in control_transfer. . .\n");
               return r;
            }


                          //  buf = buf+ChunkSize;
                             ptr = ptr + ChunkSize;
                                BlockSize -= r;
                Sum += r;
                                if(Sum == size)
                                Done = 1;
    printf("\nsum =  %d\n", Sum);

    }


    sleep(1);


                reset = 1;
                        r = cyusb_control_transfer(h, 0x40, 0xA0, 0xE600, 0x00, &reset, 0x01, 1000);

                reset = 0;
                        r = cyusb_control_transfer(h, 0x40, 0xA0, 0xE600, 0x00, &reset, 0x01, 1000);
   
    sleep(2);



    if(Done == 1){
    return 1;
    free(buf);
    }
}

please help me i want to get out of this

   

Thanks in advance

   

Regards

   

Rohaan

1 Reply
Anonymous
Not applicable
        Hi, Please create a tech support case. One of our engineers can take a look at the same. Regards, Gayathri   
0 Likes