Hello!
I want to implement UVC using FX3 (trying on SuperSpeed Kit). There is no problem with UVC examples from SDK, but I have no luck to modify USBVideoClass example to work with uncompressed frames. I've downloaded specs from USB.org - USB Device Class Specifications and changed format and frame descriptors as described. I've also changed Probe and Commit control structs.
Is there any example of FRAME_UNCOMPRESSED video translation?
v4l2-ctl output:
v4l2-ctl --all -d0
Driver Info (not using libv4l2):
Driver name : uvcvideo
Card type : FX3
Bus info : usb-0000:00:14.0-5
Driver version: 4.15.18
Capabilities : 0x84200001
Video Capture
Streaming
Extended Pix Format
Device Capabilities
Device Caps : 0x04200001
Video Capture
Streaming
Extended Pix Format
Priority: 2
Video input : 0 (Camera 1: ok)
Format Video Capture:
Width/Height : 32/24
Pixel Format : 'BGR3'
Field : None
Bytes per Line : 96
Size Image : 2304
Colorspace : Default
Transfer Function : Default (maps to Rec. 709)
YCbCr/HSV Encoding: Default (maps to ITU-R 601)
Quantization : Default (maps to Full Range)
Flags :
Crop Capability Video Capture:
Bounds : Left 0, Top 0, Width 32, Height 24
Default : Left 0, Top 0, Width 32, Height 24
Pixel Aspect: 1/1
Selection: crop_default, Left 0, Top 0, Width 32, Height 24
Selection: crop_bounds, Left 0, Top 0, Width 32, Height 24
Streaming Parameters Video Capture:
Capabilities : timeperframe
Frames per second: 25.000 (25/1)
Read buffers : 0
I'm using guvcview utility to check results. And here is the log:
...
V4L2_CORE: (get_v4l2_frame) video stream must be started first
V4L2_CORE: (get_v4l2_frame) video stream must be started first
V4L2_CORE: (get_v4l2_frame) video stream must be started first
V4L2_CORE: (get_v4l2_frame) video stream must be started first
...
lsusb output:
Bus 001 Device 047: ID 04b4:4722 Cypress Semiconductor Corp.
Device Descriptor:
bLength 18
bDescriptorType 1
bcdUSB 2.10
bDeviceClass 239 Miscellaneous Device
bDeviceSubClass 2 ?
bDeviceProtocol 1 Interface Association
bMaxPacketSize0 64
idVendor 0x04b4 Cypress Semiconductor Corp.
idProduct 0x4722
bcdDevice 0.00
iManufacturer 1 Cypress
iProduct 2 FX3
iSerial 0
bNumConfigurations 1
Configuration Descriptor:
bLength 9
bDescriptorType 2
wTotalLength 198
bNumInterfaces 2
bConfigurationValue 1
iConfiguration 0
bmAttributes 0x80
(Bus Powered)
MaxPower 400mA
Interface Association:
bLength 8
bDescriptorType 11
bFirstInterface 0
bInterfaceCount 2
bFunctionClass 14 Video
bFunctionSubClass 3 Video Interface Collection
bFunctionProtocol 0
iFunction 0
Interface Descriptor:
bLength 9
bDescriptorType 4
bInterfaceNumber 0
bAlternateSetting 0
bNumEndpoints 1
bInterfaceClass 14 Video
bInterfaceSubClass 1 Video Control
bInterfaceProtocol 0
iInterface 0
VideoControl Interface Descriptor:
bLength 13
bDescriptorType 36
bDescriptorSubtype 1 (HEADER)
bcdUVC 1.00
wTotalLength 80
dwClockFrequency 48.000000MHz
bInCollection 1
baInterfaceNr( 0) 1
VideoControl Interface Descriptor:
bLength 18
bDescriptorType 36
bDescriptorSubtype 2 (INPUT_TERMINAL)
bTerminalID 1
wTerminalType 0x0201 Camera Sensor
bAssocTerminal 0
iTerminal 0
wObjectiveFocalLengthMin 0
wObjectiveFocalLengthMax 0
wOcularFocalLength 0
bControlSize 3
bmControls 0x00000000
VideoControl Interface Descriptor:
bLength 12
bDescriptorType 36
bDescriptorSubtype 5 (PROCESSING_UNIT)
Warning: Descriptor too short
bUnitID 2
bSourceID 1
wMaxMultiplier 16384
bControlSize 3
bmControls 0x00000000
iProcessing 0
bmVideoStandards 0x1c
PAL - 625/50
SECAM - 625/50
NTSC - 625/50
VideoControl Interface Descriptor:
bLength 28
bDescriptorType 36
bDescriptorSubtype 6 (EXTENSION_UNIT)
bUnitID 3
guidExtensionCode {ffffffff-ffff-ffff-ffff-ffffffffffff}
bNumControl 0
bNrPins 1
baSourceID( 0) 2
bControlSize 3
bmControls( 0) 0x00
bmControls( 1) 0x00
bmControls( 2) 0x00
iExtension 0
VideoControl Interface Descriptor:
bLength 9
bDescriptorType 36
bDescriptorSubtype 3 (OUTPUT_TERMINAL)
bTerminalID 4
wTerminalType 0x0101 USB Streaming
bAssocTerminal 0
bSourceID 3
iTerminal 0
Endpoint Descriptor:
bLength 7
bDescriptorType 5
bEndpointAddress 0x82 EP 2 IN
bmAttributes 3
Transfer Type Interrupt
Synch Type None
Usage Type Data
wMaxPacketSize 0x0040 1x 64 bytes
bInterval 8
Interface Descriptor:
bLength 9
bDescriptorType 4
bInterfaceNumber 1
bAlternateSetting 0
bNumEndpoints 0
bInterfaceClass 14 Video
bInterfaceSubClass 2 Video Streaming
bInterfaceProtocol 0
iInterface 0
VideoStreaming Interface Descriptor:
bLength 14
bDescriptorType 36
bDescriptorSubtype 1 (INPUT_HEADER)
bNumFormats 1
wTotalLength 71
bEndPointAddress 131
bmInfo 0
bTerminalLink 4
bStillCaptureMethod 1
bTriggerSupport 1
bTriggerUsage 0
bControlSize 1
bmaControls( 0) 27
VideoStreaming Interface Descriptor:
bLength 27
bDescriptorType 36
bDescriptorSubtype 4 (FORMAT_UNCOMPRESSED)
bFormatIndex 1
bNumFrameDescriptors 1
guidFormat {7deb36e4-4f52-ce11-9f53-0020af0ba770}
bBitsPerPixel 24
bDefaultFrameIndex 1
bAspectRatioX 0
bAspectRatioY 0
bmInterlaceFlags 0x00
Interlaced stream or variable: No
Fields per frame: 2 fields
Field 1 first: No
Field pattern: Field 1 only
bCopyProtect 0
VideoStreaming Interface Descriptor:
bLength 30
bDescriptorType 36
bDescriptorSubtype 5 (FRAME_UNCOMPRESSED)
bFrameIndex 1
bmCapabilities 0x00
Still image unsupported
wWidth 32
wHeight 24
dwMinBitRate 460800
dwMaxBitRate 921600
dwMaxVideoFrameBufferSize 2304
dwDefaultFrameInterval 400000
bFrameIntervalType 1
dwFrameInterval( 0) 400000
Binary Object Store Descriptor:
bLength 5
bDescriptorType 15
wTotalLength 22
bNumDeviceCaps 2
USB 2.0 Extension Device Capability:
bLength 7
bDescriptorType 16
bDevCapabilityType 2
bmAttributes 0x00000002
Link Power Management (LPM) Supported
SuperSpeed USB Device Capability:
bLength 10
bDescriptorType 16
bDevCapabilityType 3
bmAttributes 0x00
wSpeedsSupported 0x000e
Device can operate at Full Speed (12Mbps)
Device can operate at High Speed (480Mbps)
Device can operate at SuperSpeed (5Gbps)
bFunctionalitySupport 3
Lowest fully-functional device speed is SuperSpeed (5Gbps)
bU1DevExitLat 0 micro seconds
bU2DevExitLat 0 micro seconds
Device Status: 0x0000
(Bus Powered)
Solved! Go to Solution.
Hi,
Please try to stream the video using example firmware that comes along with the FX3SDK "C:\Program Files (x86)\Cypress\EZ-USB FX3 SDK\1.3\firmware\uvc_examples\cyfxuvcinmem" and share the the result.
Have you installed the "v4l2_utils" on the PC?
If still its not working try to change descriptors in AN75779 according to your image sensor & video requirement.
Thanks & Regards
Abhinav