Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

USB low-full-high speed peripherals

Anonymous
Not applicable

Hello!

I want to implement UVC using FX3 (trying on SuperSpeed Kit). There is no problem with UVC examples from SDK, but I have no luck to modify USBVideoClass example to work with uncompressed frames. I've downloaded specs from USB.org - USB Device Class Specifications and changed format and frame descriptors as described. I've also changed Probe and Commit control structs.

Is there any example of FRAME_UNCOMPRESSED video translation?

v4l2-ctl output:

v4l2-ctl --all -d0

Driver Info (not using libv4l2):

Driver name   : uvcvideo

Card type     : FX3

Bus info      : usb-0000:00:14.0-5

Driver version: 4.15.18

Capabilities  : 0x84200001

Video Capture

Streaming

Extended Pix Format

Device Capabilities

Device Caps   : 0x04200001

Video Capture

Streaming

Extended Pix Format

Priority: 2

Video input : 0 (Camera 1: ok)

Format Video Capture:

Width/Height      : 32/24

Pixel Format      : 'BGR3'

Field             : None

Bytes per Line    : 96

Size Image        : 2304

Colorspace        : Default

Transfer Function : Default (maps to Rec. 709)

YCbCr/HSV Encoding: Default (maps to ITU-R 601)

Quantization      : Default (maps to Full Range)

Flags             :

Crop Capability Video Capture:

Bounds      : Left 0, Top 0, Width 32, Height 24

Default     : Left 0, Top 0, Width 32, Height 24

Pixel Aspect: 1/1

Selection: crop_default, Left 0, Top 0, Width 32, Height 24

Selection: crop_bounds, Left 0, Top 0, Width 32, Height 24

Streaming Parameters Video Capture:

Capabilities     : timeperframe

Frames per second: 25.000 (25/1)

Read buffers     : 0

I'm using guvcview utility to check results. And here is the log:

...

V4L2_CORE: (get_v4l2_frame) video stream must be started first

V4L2_CORE: (get_v4l2_frame) video stream must be started first

V4L2_CORE: (get_v4l2_frame) video stream must be started first

V4L2_CORE: (get_v4l2_frame) video stream must be started first

...

lsusb output:

Bus 001 Device 047: ID 04b4:4722 Cypress Semiconductor Corp.

Device Descriptor:

  bLength                18

  bDescriptorType         1

  bcdUSB               2.10

  bDeviceClass          239 Miscellaneous Device

  bDeviceSubClass         2 ?

  bDeviceProtocol         1 Interface Association

  bMaxPacketSize0        64

  idVendor           0x04b4 Cypress Semiconductor Corp.

  idProduct          0x4722

  bcdDevice            0.00

  iManufacturer           1 Cypress

  iProduct                2 FX3

  iSerial                 0

  bNumConfigurations      1

  Configuration Descriptor:

    bLength                 9

    bDescriptorType         2

    wTotalLength          198

    bNumInterfaces          2

    bConfigurationValue     1

    iConfiguration          0

    bmAttributes         0x80

      (Bus Powered)

    MaxPower              400mA

    Interface Association:

      bLength                 8

      bDescriptorType        11

      bFirstInterface         0

      bInterfaceCount         2

      bFunctionClass         14 Video

      bFunctionSubClass       3 Video Interface Collection

      bFunctionProtocol       0

      iFunction               0

    Interface Descriptor:

      bLength                 9

      bDescriptorType         4

      bInterfaceNumber        0

      bAlternateSetting       0

      bNumEndpoints           1

      bInterfaceClass        14 Video

      bInterfaceSubClass      1 Video Control

      bInterfaceProtocol      0

      iInterface              0

      VideoControl Interface Descriptor:

        bLength                13

        bDescriptorType        36

        bDescriptorSubtype      1 (HEADER)

        bcdUVC               1.00

        wTotalLength           80

        dwClockFrequency       48.000000MHz

        bInCollection           1

        baInterfaceNr( 0)       1

      VideoControl Interface Descriptor:

        bLength                18

        bDescriptorType        36

        bDescriptorSubtype      2 (INPUT_TERMINAL)

        bTerminalID             1

        wTerminalType      0x0201 Camera Sensor

        bAssocTerminal          0

        iTerminal               0

        wObjectiveFocalLengthMin      0

        wObjectiveFocalLengthMax      0

        wOcularFocalLength            0

        bControlSize                  3

        bmControls           0x00000000

      VideoControl Interface Descriptor:

        bLength                12

        bDescriptorType        36

        bDescriptorSubtype      5 (PROCESSING_UNIT)

      Warning: Descriptor too short

        bUnitID                 2

        bSourceID               1

        wMaxMultiplier      16384

        bControlSize            3

        bmControls     0x00000000

        iProcessing             0

        bmVideoStandards     0x1c

          PAL - 625/50

          SECAM - 625/50

          NTSC - 625/50

      VideoControl Interface Descriptor:

        bLength                28

        bDescriptorType        36

        bDescriptorSubtype      6 (EXTENSION_UNIT)

        bUnitID                 3

        guidExtensionCode         {ffffffff-ffff-ffff-ffff-ffffffffffff}

        bNumControl             0

        bNrPins                 1

        baSourceID( 0)          2

        bControlSize            3

        bmControls( 0)       0x00

        bmControls( 1)       0x00

        bmControls( 2)       0x00

        iExtension              0

      VideoControl Interface Descriptor:

        bLength                 9

        bDescriptorType        36

        bDescriptorSubtype      3 (OUTPUT_TERMINAL)

        bTerminalID             4

        wTerminalType      0x0101 USB Streaming

        bAssocTerminal          0

        bSourceID               3

        iTerminal               0

      Endpoint Descriptor:

        bLength                 7

        bDescriptorType         5

        bEndpointAddress     0x82  EP 2 IN

        bmAttributes            3

          Transfer Type            Interrupt

          Synch Type               None

          Usage Type               Data

        wMaxPacketSize     0x0040  1x 64 bytes

        bInterval               8

    Interface Descriptor:

      bLength                 9

      bDescriptorType         4

      bInterfaceNumber        1

      bAlternateSetting       0

      bNumEndpoints           0

      bInterfaceClass        14 Video

      bInterfaceSubClass      2 Video Streaming

      bInterfaceProtocol      0

      iInterface              0

      VideoStreaming Interface Descriptor:

        bLength                            14

        bDescriptorType                    36

        bDescriptorSubtype                  1 (INPUT_HEADER)

        bNumFormats                         1

        wTotalLength                       71

        bEndPointAddress                  131

        bmInfo                              0

        bTerminalLink                       4

        bStillCaptureMethod                 1

        bTriggerSupport                     1

        bTriggerUsage                       0

        bControlSize                        1

        bmaControls( 0)                    27

      VideoStreaming Interface Descriptor:

        bLength                            27

        bDescriptorType                    36

        bDescriptorSubtype                  4 (FORMAT_UNCOMPRESSED)

        bFormatIndex                        1

        bNumFrameDescriptors                1

        guidFormat                            {7deb36e4-4f52-ce11-9f53-0020af0ba770}

        bBitsPerPixel                      24

        bDefaultFrameIndex                  1

        bAspectRatioX                       0

        bAspectRatioY                       0

        bmInterlaceFlags                 0x00

          Interlaced stream or variable: No

          Fields per frame: 2 fields

          Field 1 first: No

          Field pattern: Field 1 only

          bCopyProtect                      0

      VideoStreaming Interface Descriptor:

        bLength                            30

        bDescriptorType                    36

        bDescriptorSubtype                  5 (FRAME_UNCOMPRESSED)

        bFrameIndex                         1

        bmCapabilities                   0x00

          Still image unsupported

        wWidth                             32

        wHeight                            24

        dwMinBitRate                   460800

        dwMaxBitRate                   921600

        dwMaxVideoFrameBufferSize        2304

        dwDefaultFrameInterval         400000

        bFrameIntervalType                  1

        dwFrameInterval( 0)            400000

Binary Object Store Descriptor:

  bLength                 5

  bDescriptorType        15

  wTotalLength           22

  bNumDeviceCaps          2

  USB 2.0 Extension Device Capability:

    bLength                 7

    bDescriptorType        16

    bDevCapabilityType      2

    bmAttributes   0x00000002

      Link Power Management (LPM) Supported

  SuperSpeed USB Device Capability:

    bLength                10

    bDescriptorType        16

    bDevCapabilityType      3

    bmAttributes         0x00

    wSpeedsSupported   0x000e

      Device can operate at Full Speed (12Mbps)

      Device can operate at High Speed (480Mbps)

      Device can operate at SuperSpeed (5Gbps)

    bFunctionalitySupport   3

      Lowest fully-functional device speed is SuperSpeed (5Gbps)

    bU1DevExitLat           0 micro seconds

    bU2DevExitLat           0 micro seconds

Device Status:     0x0000

  (Bus Powered)

0 Likes
1 Solution
abhinavg_21
Moderator
Moderator 50 likes received 25 likes received 10 likes received
Moderator

Hi,

Please try to stream the video using example firmware that comes along with the FX3SDK "C:\Program Files (x86)\Cypress\EZ-USB FX3 SDK\1.3\firmware\uvc_examples\cyfxuvcinmem" and share the the result.

Have you installed the "v4l2_utils" on the PC?

If still its not working try to change descriptors in AN75779 according to your image sensor & video requirement.

Thanks & Regards

Abhinav

View solution in original post

0 Likes
3 Replies
abhinavg_21
Moderator
Moderator 50 likes received 25 likes received 10 likes received
Moderator

Hi,

The UVC example from SDK uses a pre-stored MJPEG video frames. I guess you want to stream the video frames from an image sensor. Please make certain changes in the AN 75779. This AN makes use of sensor configuration and stream image live from the sensor.

Following is the link to download AN and its code:

http://www.cypress.com/documentation/application-notes/an75779-how-implement-image-sensor-interface-...

Thanks & Regards

Abhinav

Anonymous
Not applicable

Thank you for very useful example! My descriptors are very similar to one from AN 75779. And I can't see any error in mine.

Here is dmesg output with uvcvideo debug enabled:

[1635852.910451] usb 1-1: new high-speed USB device number 60 using xhci_hcd
[1635853.059635] usb 1-1: New USB device found, idVendor=04b4, idProduct=4722
[1635853.059641] usb 1-1: New USB device strings: Mfr=1, Product=2, SerialNumber=0
[1635853.059645] usb 1-1: Product: FX3
[1635853.059649] usb 1-1: Manufacturer: Cypress
[1635853.060257] uvcvideo: Probing generic UVC device 1
[1635853.060265] uvcvideo: Found format BGR 8:8:8 (BGR3).
[1635853.060268] uvcvideo: - 32x24 (25.0 fps)
[1635853.060278] uvcvideo: Found a Status endpoint (addr 82).
[1635853.060281] uvcvideo: Found UVC 1.00 device FX3 (04b4:4722)
[1635853.060286] uvcvideo: Scanning UVC chain: OT 4 <- XU 3 <- PU 2 <- IT 1
[1635853.060297] uvcvideo: Found a valid video chain (1 -> 4).
[1635853.060805] uvcvideo 1-1:1.0: Entity type for entity Extension 3 was not initialized!
[1635853.060810] uvcvideo 1-1:1.0: Entity type for entity Processing 2 was not initialized!
[1635853.060814] uvcvideo 1-1:1.0: Entity type for entity Camera 1 was not initialized!
[1635853.060995] input: FX3 as /devices/pci0000:00/0000:00:14.0/usb1/1-1/1-1:1.0/input/input86
[1635853.061142] uvcvideo: UVC device initialized.
[1635853.121282] uvcvideo: uvc_v4l2_open
[1635853.121333] uvcvideo: uvc_v4l2_release
[1635853.123896] uvcvideo: uvc_v4l2_open
[1635853.123905] uvcvideo: uvc_v4l2_release
[1635853.124058] uvcvideo: uvc_v4l2_open
[1635853.124063] uvcvideo: Control 0x00980900 not found.
[1635853.124064] uvcvideo: Control 0x00980901 not found.
[1635853.124065] uvcvideo: Control 0x00980902 not found.
[1635853.124065] uvcvideo: Control 0x00980903 not found.
...
[1635853.124087] uvcvideo: Control 0x00980928 not found.
[1635853.124087] uvcvideo: Control 0x00980929 not found.
[1635853.124088] uvcvideo: Control 0x0098092a not found.
[1635853.124088] uvcvideo: Control 0x08000000 not found.
[1635853.124089] uvcvideo: uvc_v4l2_release
[1635853.124657] uvcvideo: uvc_v4l2_open
[1635853.124664] uvcvideo: uvc_v4l2_release
[1635858.910488] uvcvideo: Suspending interface 1
[1635858.910491] uvcvideo: Suspending interface 0
[1635903.112139] uvcvideo: uvc_v4l2_open
[1635903.226947] uvcvideo: Resuming interface 0
[1635903.226950] uvcvideo: Resuming interface 1
[1635903.227933] uvcvideo: uvc_v4l2_release
[1635903.228683] uvcvideo: uvc_v4l2_open
[1635903.229727] uvcvideo: Control 0x00980900 not found.
[1635903.229732] uvcvideo: Control 0x00980901 not found.
[1635903.229735] uvcvideo: Control 0x00980902 not found.
[1635903.229739] uvcvideo: Control 0x00980903 not found.
...
[1635903.229969] uvcvideo: Control 0x009a091d not found.
[1635903.229972] uvcvideo: Control 0x009a091e not found.
[1635903.229976] uvcvideo: Control 0x009a091f not found.
[1635903.229979] uvcvideo: Control 0x08000000 not found.
[1635903.389051] uvcvideo: Trying format 0x33524742 (BGR3): 32x24.
[1635903.389052] uvcvideo: Using default frame interval 40000.0 us (25.0 fps).
[1635903.389671] uvcvideo: uvc_v4l2_mmap
[1635903.389674] uvcvideo: uvc_v4l2_mmap
[1635903.389676] uvcvideo: uvc_v4l2_mmap
[1635903.389678] uvcvideo: uvc_v4l2_mmap
[1635903.389684] uvcvideo: Setting frame interval to 1/25 (400000).
[1635903.909757] uvcvideo: Setting frame interval to 1/25 (400000).
[1635908.931445] uvcvideo: uvc_v4l2_release
[1635910.934850] uvcvideo: Suspending interface 1
[1635910.934853] uvcvideo: Suspending interface 0

Could you tell what is going wrong with my firmware?

0 Likes
abhinavg_21
Moderator
Moderator 50 likes received 25 likes received 10 likes received
Moderator

Hi,

Please try to stream the video using example firmware that comes along with the FX3SDK "C:\Program Files (x86)\Cypress\EZ-USB FX3 SDK\1.3\firmware\uvc_examples\cyfxuvcinmem" and share the the result.

Have you installed the "v4l2_utils" on the PC?

If still its not working try to change descriptors in AN75779 according to your image sensor & video requirement.

Thanks & Regards

Abhinav

0 Likes