Hello!
I want to implement UVC using FX3 (trying on SuperSpeed Kit). There is no problem with UVC examples from SDK, but I have no luck to modify USBVideoClass example to work with uncompressed frames. I've downloaded specs from USB.org - USB Device Class Specifications and changed format and frame descriptors as described. I've also changed Probe and Commit control structs.
Is there any example of FRAME_UNCOMPRESSED video translation?
v4l2-ctl output:
v4l2-ctl --all -d0
Driver Info (not using libv4l2):
Driver name : uvcvideo
Card type : FX3
Bus info : usb-0000:00:14.0-5
Driver version: 4.15.18
Capabilities : 0x84200001
Video Capture
Streaming
Extended Pix Format
Device Capabilities
Device Caps : 0x04200001
Video Capture
Streaming
Extended Pix Format
Priority: 2
Video input : 0 (Camera 1: ok)
Format Video Capture:
Width/Height : 32/24
Pixel Format : 'BGR3'
Field : None
Bytes per Line : 96
Size Image : 2304
Colorspace : Default
Transfer Function : Default (maps to Rec. 709)
YCbCr/HSV Encoding: Default (maps to ITU-R 601)
Quantization : Default (maps to Full Range)
Flags :
Crop Capability Video Capture:
Bounds : Left 0, Top 0, Width 32, Height 24
Default : Left 0, Top 0, Width 32, Height 24
Pixel Aspect: 1/1
Selection: crop_default, Left 0, Top 0, Width 32, Height 24
Selection: crop_bounds, Left 0, Top 0, Width 32, Height 24
Streaming Parameters Video Capture:
Capabilities : timeperframe
Frames per second: 25.000 (25/1)
Read buffers : 0
I'm using guvcview utility to check results. And here is the log:
...
V4L2_CORE: (get_v4l2_frame) video stream must be started first
V4L2_CORE: (get_v4l2_frame) video stream must be started first
V4L2_CORE: (get_v4l2_frame) video stream must be started first
V4L2_CORE: (get_v4l2_frame) video stream must be started first
...
lsusb output:
Bus 001 Device 047: ID 04b4:4722 Cypress Semiconductor Corp.
Device Descriptor:
bLength 18
bDescriptorType 1
bcdUSB 2.10
bDeviceClass 239 Miscellaneous Device
bDeviceSubClass 2 ?
bDeviceProtocol 1 Interface Association
bMaxPacketSize0 64
idVendor 0x04b4 Cypress Semiconductor Corp.
idProduct 0x4722
bcdDevice 0.00
iManufacturer 1 Cypress
iProduct 2 FX3
iSerial 0
bNumConfigurations 1
Configuration Descriptor:
bLength 9
bDescriptorType 2
wTotalLength 198
bNumInterfaces 2
bConfigurationValue 1
iConfiguration 0
bmAttributes 0x80
(Bus Powered)
MaxPower 400mA
Interface Association:
bLength 8
bDescriptorType 11
bFirstInterface 0
bInterfaceCount 2
bFunctionClass 14 Video
bFunctionSubClass 3 Video Interface Collection
bFunctionProtocol 0
iFunction 0
Interface Descriptor:
bLength 9
bDescriptorType 4
bInterfaceNumber 0
bAlternateSetting 0
bNumEndpoints 1
bInterfaceClass 14 Video
bInterfaceSubClass 1 Video Control
bInterfaceProtocol 0
iInterface 0
VideoControl Interface Descriptor:
bLength 13
bDescriptorType 36
bDescriptorSubtype 1 (HEADER)
bcdUVC 1.00
wTotalLength 80
dwClockFrequency 48.000000MHz
bInCollection 1
baInterfaceNr( 0) 1
VideoControl Interface Descriptor:
bLength 18
bDescriptorType 36
bDescriptorSubtype 2 (INPUT_TERMINAL)
bTerminalID 1
wTerminalType 0x0201 Camera Sensor
bAssocTerminal 0
iTerminal 0
wObjectiveFocalLengthMin 0
wObjectiveFocalLengthMax 0
wOcularFocalLength 0
bControlSize 3
bmControls 0x00000000
VideoControl Interface Descriptor:
bLength 12
bDescriptorType 36
bDescriptorSubtype 5 (PROCESSING_UNIT)
Warning: Descriptor too short
bUnitID 2
bSourceID 1
wMaxMultiplier 16384
bControlSize 3
bmControls 0x00000000
iProcessing 0
bmVideoStandards 0x1c
PAL - 625/50
SECAM - 625/50
NTSC - 625/50
VideoControl Interface Descriptor:
bLength 28
bDescriptorType 36
bDescriptorSubtype 6 (EXTENSION_UNIT)
bUnitID 3
guidExtensionCode {ffffffff-ffff-ffff-ffff-ffffffffffff}
bNumControl 0
bNrPins 1
baSourceID( 0) 2
bControlSize 3
bmControls( 0) 0x00
bmControls( 1) 0x00
bmControls( 2) 0x00
iExtension 0
VideoControl Interface Descriptor:
bLength 9
bDescriptorType 36
bDescriptorSubtype 3 (OUTPUT_TERMINAL)
bTerminalID 4
wTerminalType 0x0101 USB Streaming
bAssocTerminal 0
bSourceID 3
iTerminal 0
Endpoint Descriptor:
bLength 7
bDescriptorType 5
bEndpointAddress 0x82 EP 2 IN
bmAttributes 3
Transfer Type Interrupt
Synch Type None
Usage Type Data
wMaxPacketSize 0x0040 1x 64 bytes
bInterval 8
Interface Descriptor:
bLength 9
bDescriptorType 4
bInterfaceNumber 1
bAlternateSetting 0
bNumEndpoints 0
bInterfaceClass 14 Video
bInterfaceSubClass 2 Video Streaming
bInterfaceProtocol 0
iInterface 0
VideoStreaming Interface Descriptor:
bLength 14
bDescriptorType 36
bDescriptorSubtype 1 (INPUT_HEADER)
bNumFormats 1
wTotalLength 71
bEndPointAddress 131
bmInfo 0
bTerminalLink 4
bStillCaptureMethod 1
bTriggerSupport 1
bTriggerUsage 0
bControlSize 1
bmaControls( 0) 27
VideoStreaming Interface Descriptor:
bLength 27
bDescriptorType 36
bDescriptorSubtype 4 (FORMAT_UNCOMPRESSED)
bFormatIndex 1
bNumFrameDescriptors 1
guidFormat {7deb36e4-4f52-ce11-9f53-0020af0ba770}
bBitsPerPixel 24
bDefaultFrameIndex 1
bAspectRatioX 0
bAspectRatioY 0
bmInterlaceFlags 0x00
Interlaced stream or variable: No
Fields per frame: 2 fields
Field 1 first: No
Field pattern: Field 1 only
bCopyProtect 0
VideoStreaming Interface Descriptor:
bLength 30
bDescriptorType 36
bDescriptorSubtype 5 (FRAME_UNCOMPRESSED)
bFrameIndex 1
bmCapabilities 0x00
Still image unsupported
wWidth 32
wHeight 24
dwMinBitRate 460800
dwMaxBitRate 921600
dwMaxVideoFrameBufferSize 2304
dwDefaultFrameInterval 400000
bFrameIntervalType 1
dwFrameInterval( 0) 400000
Binary Object Store Descriptor:
bLength 5
bDescriptorType 15
wTotalLength 22
bNumDeviceCaps 2
USB 2.0 Extension Device Capability:
bLength 7
bDescriptorType 16
bDevCapabilityType 2
bmAttributes 0x00000002
Link Power Management (LPM) Supported
SuperSpeed USB Device Capability:
bLength 10
bDescriptorType 16
bDevCapabilityType 3
bmAttributes 0x00
wSpeedsSupported 0x000e
Device can operate at Full Speed (12Mbps)
Device can operate at High Speed (480Mbps)
Device can operate at SuperSpeed (5Gbps)
bFunctionalitySupport 3
Lowest fully-functional device speed is SuperSpeed (5Gbps)
bU1DevExitLat 0 micro seconds
bU2DevExitLat 0 micro seconds
Device Status: 0x0000
(Bus Powered)
Solved! Go to Solution.
Hi,
Please try to stream the video using example firmware that comes along with the FX3SDK "C:\Program Files (x86)\Cypress\EZ-USB FX3 SDK\1.3\firmware\uvc_examples\cyfxuvcinmem" and share the the result.
Have you installed the "v4l2_utils" on the PC?
If still its not working try to change descriptors in AN75779 according to your image sensor & video requirement.
Thanks & Regards
Abhinav
Hi,
The UVC example from SDK uses a pre-stored MJPEG video frames. I guess you want to stream the video frames from an image sensor. Please make certain changes in the AN 75779. This AN makes use of sensor configuration and stream image live from the sensor.
Following is the link to download AN and its code:
Thanks & Regards
Abhinav
Thank you for very useful example! My descriptors are very similar to one from AN 75779. And I can't see any error in mine.
Here is dmesg output with uvcvideo debug enabled:
[1635852.910451] usb 1-1: new high-speed USB device number 60 using xhci_hcd
[1635853.059635] usb 1-1: New USB device found, idVendor=04b4, idProduct=4722
[1635853.059641] usb 1-1: New USB device strings: Mfr=1, Product=2, SerialNumber=0
[1635853.059645] usb 1-1: Product: FX3
[1635853.059649] usb 1-1: Manufacturer: Cypress
[1635853.060257] uvcvideo: Probing generic UVC device 1
[1635853.060265] uvcvideo: Found format BGR 8:8:8 (BGR3).
[1635853.060268] uvcvideo: - 32x24 (25.0 fps)
[1635853.060278] uvcvideo: Found a Status endpoint (addr 82).
[1635853.060281] uvcvideo: Found UVC 1.00 device FX3 (04b4:4722)
[1635853.060286] uvcvideo: Scanning UVC chain: OT 4 <- XU 3 <- PU 2 <- IT 1
[1635853.060297] uvcvideo: Found a valid video chain (1 -> 4).
[1635853.060805] uvcvideo 1-1:1.0: Entity type for entity Extension 3 was not initialized!
[1635853.060810] uvcvideo 1-1:1.0: Entity type for entity Processing 2 was not initialized!
[1635853.060814] uvcvideo 1-1:1.0: Entity type for entity Camera 1 was not initialized!
[1635853.060995] input: FX3 as /devices/pci0000:00/0000:00:14.0/usb1/1-1/1-1:1.0/input/input86
[1635853.061142] uvcvideo: UVC device initialized.
[1635853.121282] uvcvideo: uvc_v4l2_open
[1635853.121333] uvcvideo: uvc_v4l2_release
[1635853.123896] uvcvideo: uvc_v4l2_open
[1635853.123905] uvcvideo: uvc_v4l2_release
[1635853.124058] uvcvideo: uvc_v4l2_open
[1635853.124063] uvcvideo: Control 0x00980900 not found.
[1635853.124064] uvcvideo: Control 0x00980901 not found.
[1635853.124065] uvcvideo: Control 0x00980902 not found.
[1635853.124065] uvcvideo: Control 0x00980903 not found.
...
[1635853.124087] uvcvideo: Control 0x00980928 not found.
[1635853.124087] uvcvideo: Control 0x00980929 not found.
[1635853.124088] uvcvideo: Control 0x0098092a not found.
[1635853.124088] uvcvideo: Control 0x08000000 not found.
[1635853.124089] uvcvideo: uvc_v4l2_release
[1635853.124657] uvcvideo: uvc_v4l2_open
[1635853.124664] uvcvideo: uvc_v4l2_release
[1635858.910488] uvcvideo: Suspending interface 1
[1635858.910491] uvcvideo: Suspending interface 0
[1635903.112139] uvcvideo: uvc_v4l2_open
[1635903.226947] uvcvideo: Resuming interface 0
[1635903.226950] uvcvideo: Resuming interface 1
[1635903.227933] uvcvideo: uvc_v4l2_release
[1635903.228683] uvcvideo: uvc_v4l2_open
[1635903.229727] uvcvideo: Control 0x00980900 not found.
[1635903.229732] uvcvideo: Control 0x00980901 not found.
[1635903.229735] uvcvideo: Control 0x00980902 not found.
[1635903.229739] uvcvideo: Control 0x00980903 not found.
...
[1635903.229969] uvcvideo: Control 0x009a091d not found.
[1635903.229972] uvcvideo: Control 0x009a091e not found.
[1635903.229976] uvcvideo: Control 0x009a091f not found.
[1635903.229979] uvcvideo: Control 0x08000000 not found.
[1635903.389051] uvcvideo: Trying format 0x33524742 (BGR3): 32x24.
[1635903.389052] uvcvideo: Using default frame interval 40000.0 us (25.0 fps).
[1635903.389671] uvcvideo: uvc_v4l2_mmap
[1635903.389674] uvcvideo: uvc_v4l2_mmap
[1635903.389676] uvcvideo: uvc_v4l2_mmap
[1635903.389678] uvcvideo: uvc_v4l2_mmap
[1635903.389684] uvcvideo: Setting frame interval to 1/25 (400000).
[1635903.909757] uvcvideo: Setting frame interval to 1/25 (400000).
[1635908.931445] uvcvideo: uvc_v4l2_release
[1635910.934850] uvcvideo: Suspending interface 1
[1635910.934853] uvcvideo: Suspending interface 0
Could you tell what is going wrong with my firmware?
Hi,
Please try to stream the video using example firmware that comes along with the FX3SDK "C:\Program Files (x86)\Cypress\EZ-USB FX3 SDK\1.3\firmware\uvc_examples\cyfxuvcinmem" and share the the result.
Have you installed the "v4l2_utils" on the PC?
If still its not working try to change descriptors in AN75779 according to your image sensor & video requirement.
Thanks & Regards
Abhinav