Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
Anonymous
Not applicable

I have a 3 button mouse working (with PSoC 1 device- CY8C24894), but I would like to add the wheel functionality to it. I would appreciate if anyone can share some info on this. I have modified the HID Template (for the 3 button mouse), but for some reason the mouse does not work at all with this configuration after modification, so I would assume that there is something wrong with what I am doing.

0 Likes
3 Replies
Anonymous
Not applicable
0 Likes
Anonymous
Not applicable

 I got the wheel mouse working after looking at the microsoft wheel.docx at http://msdn.microsoft.com/en-us/windows/hardware/gg487477.aspx

   

And this post at microchip forum, http://www.microchip.com/forums/tm.aspx?m=391435

   

If someone is looking for it, here is a simplified report descriptor which can be used to create a HID Report template in PSoC Designer.

   

   
 char ReportDescriptor[118] = {
     
0x05, 0x01,        // USAGE_PAGE (Generic Desktop)
     
0x09, 0x02,        // USAGE (Mouse)
     
0xa1, 0x01,        // COLLECTION (Application)
     
0x09, 0x02,        //   USAGE (Mouse)
     
0xa1, 0x02,        //   COLLECTION (Logical)
     
0x09, 0x01,        //     USAGE (Pointer)
     
0xa1, 0x00,        //     COLLECTION (Physical)
                       
// ------------------------------  Buttons
     
0x05, 0x09,        //       USAGE_PAGE (Button)      
     
0x19, 0x01,        //       USAGE_MINIMUM (Button 1)
     
0x29, 0x05,        //       USAGE_MAXIMUM (Button 5)
     
0x15, 0x00,        //       LOGICAL_MINIMUM (0)
     
0x25, 0x01,        //       LOGICAL_MAXIMUM (1)
     
0x75, 0x01,        //       REPORT_SIZE (1)
     
0x95, 0x05,        //       REPORT_COUNT (5)
     
0x81, 0x02,        //       INPUT (Data,Var,Abs)
                       
// ------------------------------  Padding
     
0x75, 0x03,        //       REPORT_SIZE (3)
     
0x95, 0x01,        //       REPORT_COUNT (1)
     
0x81, 0x03,        //       INPUT (Cnst,Var,Abs)
                       
// ------------------------------  X,Y position
     
0x05, 0x01,        //       USAGE_PAGE (Generic Desktop)
     
0x09, 0x30,        //       USAGE (X)
     
0x09, 0x31,        //       USAGE (Y)
     
0x15, 0x81,        //       LOGICAL_MINIMUM (-127)
     
0x25, 0x7f,        //       LOGICAL_MAXIMUM (127)
     
0x75, 0x08,        //       REPORT_SIZE (8)
     
0x95, 0x02,        //       REPORT_COUNT (2)
     
0x81, 0x06,        //       INPUT (Data,Var,Rel)
     
0xa1, 0x02,        //       COLLECTION (Logical)
                       
// ------------------------------  Vertical wheel res multiplier
     
0x09, 0x48,        //         USAGE (Resolution Multiplier)
     
0x15, 0x00,        //         LOGICAL_MINIMUM (0)
     
0x25, 0x01,        //         LOGICAL_MAXIMUM (1)
     
0x35, 0x01,        //         PHYSICAL_MINIMUM (1)
     
0x45, 0x04,        //         PHYSICAL_MAXIMUM (4)
     
0x75, 0x02,        //         REPORT_SIZE (2)
     
0x95, 0x01,        //         REPORT_COUNT (1)
     
0xa4,              //         PUSH
     
0xb1, 0x02,        //         FEATURE (Data,Var,Abs)
                       
// ------------------------------  Vertical wheel
     
0x09, 0x38,        //         USAGE (Wheel)
     
0x15, 0x81,        //         LOGICAL_MINIMUM (-127)
     
0x25, 0x7f,        //         LOGICAL_MAXIMUM (127)
     
0x35, 0x00,        //         PHYSICAL_MINIMUM (0)        - reset physical
     
0x45, 0x00,        //         PHYSICAL_MAXIMUM (0)
     
0x75, 0x08,        //         REPORT_SIZE (8)
     
0x81, 0x06,        //         INPUT (Data,Var,Rel)
     
0xc0,              //       END_COLLECTION
     
0xa1, 0x02,        //       COLLECTION (Logical)
                       
// ------------------------------  Horizontal wheel res multiplier
     
0x09, 0x48,        //         USAGE (Resolution Multiplier)
     
0xb4,              //         POP
     
0xb1, 0x02,        //         FEATURE (Data,Var,Abs)
                       
// ------------------------------  Padding for Feature report
     
0x35, 0x00,        //         PHYSICAL_MINIMUM (0)        - reset physical
     
0x45, 0x00,        //         PHYSICAL_MAXIMUM (0)
     
0x75, 0x04,        //         REPORT_SIZE (4)
     
0xb1, 0x03,        //         FEATURE (Cnst,Var,Abs)
                       
// ------------------------------  Horizontal wheel
     
0x05, 0x0c,        //         USAGE_PAGE (Consumer Devices)
     
0x0a, 0x38, 0x02,  //         USAGE (AC Pan)
     
0x15, 0x81,        //         LOGICAL_MINIMUM (-127)
     
0x25, 0x7f,        //         LOGICAL_MAXIMUM (127)
     
0x75, 0x08,        //         REPORT_SIZE (8)
     
0x81, 0x06,        //         INPUT (Data,Var,Rel)
     
0xc0,              //       END_COLLECTION
     
0xc0,              //     END_COLLECTION
     
0xc0,              //   END_COLLECTION
     
0xc0               // END_COLLECTION
 
};
0 Likes
Anonymous
Not applicable

 Hi,

   

 Thank you for sharing your solution here, it will be helpful for others  who have similar questions.

   

Thanks

   

Prajith

0 Likes