Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

USB low-full-high speed peripherals

qiwec_297866
Level 2
10 questions asked 5 replies posted 5 questions asked
Level 2

 Hello!

   

    I transfer data from 68013A to cpld, using the synchronous salve fifo mode, and the data bus is 16 bit, but I can only read the first word correctly, and the second word is always the same as the first word, please help me!

   

   the next is my code.

   

   the 68013A code:

   

   void TD_Init( void )

   

{ // Called once at startup

   

 

   

  CPUCS = 0x10;                 // CLKSPD[1:0]=10, for 48MHz operation

   

    REVCTL = 0x01; // MUST set REVCTL.0 and REVCTL.1 to 1

   

    SYNCDELAY;

   

    IFCONFIG = 0x43;        //%Slave FIFO接口模式 采用外部时钟 极性正常 内部时钟输出无效 同步操作

   

  //%端点2配置,OUT,双缓冲,BULK 批量输出 数据从PC机到68013

   

  //0xA0 四缓冲 0xA2 双缓冲 0xA3 三缓冲 

   

    SYNCDELAY;

   

  EP2CFG = 0xA2;     SYNCDELAY;// EP2OUT, bulk, size 512, 2 buffered  命令输出

   

  EP4CFG = 0x02;     SYNCDELAY;// EP4 not valid

   

  EP6CFG = 0xe2;     SYNCDELAY;// EP6IN,  bulk, size 512, 2 buffered  数据输入

   

  EP8CFG = 0x02;     SYNCDELAY;// EP8 not valid

   

 

   

    //在复位端点FIFO 时,为了保证复位正常,防止主控器请求的干扰,先写入 0x80,然后复位端点,最后写入0x00,使能响应请求。

   

  FIFORESET = 0x80;    SYNCDELAY;          // activate NAK-ALL to avoid race conditions

   

  FIFORESET = 0x02;    SYNCDELAY;         // reset, FIFO 2

   

  FIFORESET = 0x04;    SYNCDELAY;         // reset, FIFO 4

   

  FIFORESET = 0x06;    SYNCDELAY;         // reset, FIFO 6

   

  FIFORESET = 0x08;    SYNCDELAY;         // reset, FIFO 8

   

  FIFORESET = 0x00;    SYNCDELAY;         // deactivate NAK-ALL

   

  //0x11 /16位数据宽度 数据自动提交 

   

    EP2FIFOCFG = 0x01;   SYNCDELAY;

   

  EP2FIFOCFG = 0x11;   SYNCDELAY;         //AUTOOUT=1, WORDWIDE=1  16位数据宽度

   

    //16位数据宽度,数据自动提交,可以提交0长度数据封包

   

  EP6FIFOCFG = 0x0D;   SYNCDELAY;         // AUTOIN=1, ZEROLENIN=1, WORDWIDE=1

   

  

   

//%引脚FLAGC、FLAGB、FLAGC、FLAGB配置

   

  PINFLAGSAB = 0x00;   SYNCDELAY;         // FLAGB - Indexed 满标志低电平有效

   

  PINFLAGSCD = 0x00;   SYNCDELAY;         // FLAGC - Indexed 空标志低电平有效

   

 

   

    //%PKEND\SLOE\SLRD\SLWR 高电平有效 空满标志低电平有效 PKTEND高电平有效,不允许短包

   

  FIFOPINPOLAR = 0x3C; SYNCDELAY;       // FLAGB/A  读写和使能 高有效     

   

 

   

    EP6AUTOINLENH = 0x02; SYNCDELAY;

   

EP6AUTOINLENL = 0x00; SYNCDELAY; //端点6数据包长度512

   

 

   

OEA |= 0x0B;

   

IOA &= 0xF4;

   

}

   

  The following is the cpld code:

   

  assign usbifclk = clk;

   

  always @(negedge clk)

   

  begin

   

  if(!rst)

   

  begin

   

    present_state <= state_idel;

   

    count_clk <= 10'd0;

   

   slrd <= 1'b0;//slrd and sloe is 1 active

   

   sloe <= 1'b0;

   

   config_done <= 1'b0;

   

   done_delay_cnt <= 3'd0;

   

   user_control_data <= 20'd0;

   

 end

   

 else

   

 begin

   

 case(present_state)

   

 state_idel :

   

 begin

   

   if((!usbfifo_full)&(usbfifo_empty))

   

   begin

   

     present_state <= state_read;

   

     slrd <= 1'b1;

   

     sloe <= 1'b1;

   

   end

   

   else if((!usbfifo_empty)&(usbfifo_full))

   

   begin

   

     present_state <= state_idel;

   

     slrd <= 1'b0;

   

     sloe <= 1'b0;

   

   end

   

 end

   

 state_read :

   

 begin

   

  if(count_clk <= 10'd511)

   

  begin

   

    count_clk <= count_clk + 1'b1;

   

    if(count_clk == 10'd511)

   

    begin

   

      slrd <= 1'b0;

   

      sloe <= 1'b0;

   

    end

   

    else

   

    begin

   

      slrd <= 1'b1;

   

      sloe <= 1'b1;

   

    end

   

    if(count_clk == 10'd0)

   

      user_control_data[15:0] <= fddata;

   

    else if(count_clk == 10'd1)

   

      user_control_data[19:16] <= fddata[3:0];

   

  end

   

  else if(count_clk == 10'd512)

   

  begin

   

    count_clk <= 10'd0;

   

    config_done <= 1'b1;

   

    present_state <= state_delay;

   

  end

   

 end

   

 state_delay :

   

 begin

   

   if(done_delay_cnt<=3'd6)

   

     done_delay_cnt <= done_delay_cnt + 1'b1;

   

   else

   

   begin

   

     config_done <= 1'b0;

   

     done_delay_cnt <= 3'd0;

   

     present_state <= state_idel;

   

   end

   

 end

   

 default :

   

   present_state <= state_idel;

   

endcase

   

end

   

end

   

  Now, the problem is that: When I send 1024 bytes through fifo2 to cpld, such as {22 2A 0B 01 01 ... 01}, the cpld can run the code and read over the full 1024 bytes, and user_control_data[15:0] is correct(22 2A), but the received user_control_data[19:16] is always the same as the user_control_data[3:0](22), How can I solve the problem? I checked the sequence diagram, the it seems does right.

0 Likes
1 Reply
Anonymous
Not applicable

 Hi,

   

 

   

SYNCDELAY;

   

   EP2CFG = 0xA2;      SYNCDELAY;// EP2OUT, bulk, size 512, 2 buffered  命令输出

   

   EP4CFG = 0x02;      SYNCDELAY;// EP4 not valid

   

   EP6CFG = 0xe2;      SYNCDELAY;// EP6IN,  bulk, size 512, 2 buffered  数据输入

   

   EP8CFG = 0x02;      SYNCDELAY;// EP8 not valid

   

 

   

this is not valid configuration for endpoints.Pls refer fugre 2.5 of datasheet for valid configuration options

   

 

   

i don't this "user_control_data[19:16] <= fddata[3:0];" What is fddata[3:0]?

   

 

   

Regards,

   

Vikas

0 Likes