Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
JeBo_4132831
Level 4
Level 4
25 replies posted 25 sign-ins 10 replies posted

OK.

After FPGA loading we use the SLAVE FIFO interface. The FPGA is the MASTER.

Behind the SLAVE FIFO there is a Finite STate Machine. This FSM wait for a COMMAND from HOST. This COMMAND is made of several bytes. It is analyzed  Then if is a READ COMMAND, the FPGA writes the ANSWER into the BUFFER and indicates to the FX2 that is must send DATA.

In your previous answer, I've not understood exactly HOW the FPGA can inform the HOST PC that is has DATA to send ?

Could you precise this ?

What we need to do in terms of PC Software ? firmware ? And FPGA side ?

Goel is to avoid doing USB POLLING like today, with a READ COMMAND.

Thanks.

0 Likes
1 Solution

Hello,

That above solution which you have mentioned will work.

For a simpler way, you can directly check the Status of the EP2 (empty/not empty)  which receives data from the FPGA, through the register EP2CS or EP2468STAT.

If the EP2 is not empty, then a read operation can be performed.

Also you can check the number of packets available in the FIFO by reading the NPAK bits of the EP2CS register.

Thanks,

Yatheesh

View solution in original post

0 Likes
3 Replies
YatheeshD_36
Moderator
Moderator
Moderator
750 replies posted 500 replies posted 250 solutions authored

Hello,

In order for the Host PC to know if there is data available in the FX2LP, It should poll the endpoint through a subsequent read commands.

For an alternate way, you can implement a vendor command through the control end point whenever needed to check the availability of data in the endpoint buffer by monitoring the EPxCS ("x" is the EP number) register after the data is committed from the FIFO, and then perform a Read transfer from the host.

In either case, polling for availability of data is needed from the host side to FX2LP.

Thanks,

Yatheesh

OK if i understand.

Today our FPGA and Firmware /Software implementation use ENDPOINT FIFO2 and 6.

FIFO6 to send command to FPGA from the HOST/PC.

FIFO2 to send DATA from the FPGA to the HOST/PC.

FIFO6 is an OUTPUT ENDPOINT.

FIFO2 is an INPUT ENDPOINT.

What you propose is to add for instance a new FIFO management.

FIFO4 for instance. As an INPUT ENDPOINT. The FPGA Fills this FIFO when needed (without any HOST request READ command).

A Specific Vendor Command need to be added in the Firmware. This specific vendor command, reads the EP4CS Empty or Full (depending of the management FPGA side) and Return a "there is DATA in the Buffer 4"  information to the HOST/PC ?

Then the HOST/PC can read the FIFO4 ENDPOINT buffer ?

This is correct ?

0 Likes

Hello,

That above solution which you have mentioned will work.

For a simpler way, you can directly check the Status of the EP2 (empty/not empty)  which receives data from the FPGA, through the register EP2CS or EP2468STAT.

If the EP2 is not empty, then a read operation can be performed.

Also you can check the number of packets available in the FIFO by reading the NPAK bits of the EP2CS register.

Thanks,

Yatheesh

0 Likes