Announcements

Learn how to optimise USB-C for your designs at 18 May's USB-C PD Webinar.
Click here to register.

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Anonymous
Not applicable

Hi
I am using cypress cy7c68013a-100a and driver cyusb.sys in "Cypress Suite USB 3.4.6"
for win 7 in wlh folder.
and change .inf file (my .inf is attached)

   

and build a board according AN15456 in this address

   

www.cypress.com/?rID=12956

   

When I connect on some PC's running Windows 7, i see "the device is not recognized" and "this device connot start(code10)"!

   

I checked my hardware again and again.but i see this error yet

   

* i can't find 'tps3820-33' for reset pin so i use a  100k from  reset pin to 3.3v and a 0.1uf to gnd *

   

'tps3820-33' is my problem?!!

   

Thanks in advance for any help you can offer

   

sam

1 Solution
Anonymous
Not applicable

Hi

   

this is my .inf file

View solution in original post

0 Likes
20 Replies
Anonymous
Not applicable

Hi

   

this is my .inf file

0 Likes
Anonymous
Not applicable

 Hi,

   

 

   

Can you just look at the device Properties being shown in the device manager and let me know what is the VID/PID being shown there. Is it the expected one? Also you forgot to attach the inf file in your previous post.

   

In your board, are you using EEPROM for loading the firmware? Or is it just the default configuration?

   

Can you just try out 100k pulled up to 3.3V, 1uF pulled down to ground at the RESET pin and let me know if it has any change.

   

Regards,

   

Gayathri

lock attach
Attachments are accessible only for community members.
Anonymous
Not applicable

Hi

   

 

   

thanks Gayathry for reply to me soon and sorry for my bad english

   


 

   

-in 'device instance path' in detail ,  i seeing " USB\VID_0000&PID_0000\5&2BCCD040&0&1"

   

 

   

i know i should  see   vid\pid :04b4 /8613 !!

   


 

   

-at first time eeprom was connected  to scl&sda pin but now these pins is connect to 3.3v by 1.1k

   

 

   

- i connect 100k pulled up to 3.3V, 1uF pulled down to ground at the RESET pin but i can't see any change

   


 

   

i have some question :

   

 

   

1)i use 24mhz crystal with two 20pf , i want to know is crystal important in this stage and what is your idea about  use a 24mhz oscillator  instead of crystal?

   


 

   

2)i use a 'lf33cv' Regulator to 3.3v .is it suitable or i must use LDO (low-dropout regulator) like the LM2937?

   


 

   

i think is better  know :

   

 

   

in first time that i plaged in "the device is not recognized" and OS recognized my device to "other device" in device manager and when install my driver ,i don't see any error and driver was installed

   

 

   

BUT for other time window recognized my device to "usb controller" and i can't install driver and see error !

   

 

   

maybe it help to you for help to me

   


 

   

thanks

   

 

   

sam

   




 

0 Likes
Anonymous
Not applicable

no body can help me!

   

please

0 Likes
Anonymous
Not applicable

 Hi,

   

Do you mean to say that when you plugged in for the first time, it initially showed up in the Other devices section, and then you were able to install the driver succesfully. In this case, after the successfull installation of the driver, did it show up as the Default FX2LP device with VID/PID of 0x04B4 / 0x8613? 

   

I hope you would have saved the the .tx file with .inf extension before trying to bind. In the failing cases, that is when you are not able to install the driver, what is the status shown in the Driver installation wizard, when it shows up" "Unable to install the driver" ?

   

Is it possible to get a CATC trace / USB trace using some other USB traffic analyzer? 

   

 

   

Regards,

   

Gayathri

0 Likes
Anonymous
Not applicable

 Hi,

   
   

 

   
   

As long as teh oscillator is able to meet the frquency criteria, that should not be a proble.

   
   

Even the regulator, I don't think can cause an issue. The preferred pull-ups on the SCL & SDA lines are 2.2k. You can just give it atry using that value. You should use separate pull-ups for both the lines.

   
   

Also routing of the USB bus is important. Please follow the guidelines in the application note from: http://www.cypress.com/?docID=25406 for a good PDB design.

   
   

 

   
   

Regards,

   
   

Gayathri

0 Likes
lock attach
Attachments are accessible only for community members.
Anonymous
Not applicable

Hi

   

thank Gayathri for your answer and sorry because of delay my reply
this is my schematic .please look at and tell me your suggestion

   

in first time than my device recognized i didnt  check VID/PID and i dont now why and when OS not recognize

   

so i change 1.1k to 2.2k but not any thing happen

   

- i try to usb trace with"USB lyzer" but i see this error : ' Connection Status:Enumeration of device failed'

   

-you can see properties window in this picture:

   

www.mediafire.com/i/

   

i see in details 

   

hardware ide:    USB\UNKNOWN
device instance path : USB\VID_0000&PID_0000\5&2BCCD040&0&1
problem code : 0000000A
deriver node strong name : oem11.inf:Device.NTx86:CyUsb:3.4.6.0:usb\vid_04b4&pid_8613
matching device ld : usb\vid_04b4&pid_8613

   

so please tell me your suggection about  this information and my .inf file 

   

and if you have a schematic or .inf file please send to me

   

thank for your help

   

sam
 

0 Likes
lock attach
Attachments are accessible only for community members.
Anonymous
Not applicable

 Hello,

   

 

   

As I went through your schematic, I noticed that the crystals are connected between the XTALOUT pin and the CLKOUT pin. It is supposed to be connected between XTALIN and XTALOUT pins. 

   

Also, I wanted to confirm that the pin9(AVCC) is connected to supply. Please try with the capacitors connected only to the AVCC pins, and VCC pins connected directly to supply. Please find the attached figure for the the connection of VCC pins and AVCC pins to supply.

   

 

   

Regards,

   

Gayathri

0 Likes
Anonymous
Not applicable

Hi

   

thanks you for prompt and perfect reply

   

i cannected avcc(9,16 pin) to caps and cannected to 3.3v with 47ohm but in OS not any thing happen so i changed resistor with a wire and see usual error(not device recognized)

   

what is your idea about my .inf file .have it any problem?and can you send me your .inf file?(if you have)

   

you tell me in Previous reply routing is important.so do you have any pcb(or schematic)?please send to me

   

 thanks alot for spending time for my problem

   

sam

0 Likes
Anonymous
Not applicable

 Hi,

   

 

   

Did you check your crystal's connection that I had pointed out in my previous response?

   

 

   

Regards,

   

Gayathri

0 Likes
Anonymous
Not applicable

Hi

   

it's a good point .but i cannected my crystal truly in my hardware and my mistake is in schematic that send to you(sorry)

   

sam

0 Likes
Anonymous
Not applicable

 Hi,

   

 

   

Please find the attached inf files. If you are using Win 7 32bit OS, please use cyusb.inf file inside wlh \ x86 folder.

   

If you are using Win7 64bit OS, please use cyusb.inf file inside wlh \ x64 folder.

   

 

   

Regards,

   

Gayathri

0 Likes
Anonymous
Not applicable

Please find the attachment.

0 Likes
Anonymous
Not applicable

 I dont know, why I am  not able to attach the zip file. Trying to attach the inf files as such.

0 Likes
Anonymous
Not applicable
0 Likes
lock attach
Attachments are accessible only for community members.
Anonymous
Not applicable
0 Likes
lock attach
Attachments are accessible only for community members.
Anonymous
Not applicable

 Sorry for the confusion. Please find the files.

0 Likes
Anonymous
Not applicable

Hi

   

i have  question.

   

i think according to cypress technical note such as" AN61465" we should change

   

((;%VID_XXXX&PID_XXXX.DeviceDesc%=CyUsb )) in .inf file with

   

((%VID_04b4&PID_8613.DeviceDesc%=CyUsb))

   

do u agree with me?

0 Likes
lock attach
Attachments are accessible only for community members.
Anonymous
Not applicable

Hi,

   

 

   

 Please find the attachment. Please change the file name extension to chm and then open it. In that, refer section Modifying CyUSB.INF.

   

 

   

Regards,

   

Gayathri

0 Likes
Anonymous
Not applicable

 Again some problem with attachment. So I am posting it here:

   

 

   

   

To make the driver match to a specific device, the device's vendor ID and product ID need to be added to the .inf file.

   

 Locate the following sections [Device],[Device.NT],[Device.Ntx86] and [Device.Ntamd64]  and remove the semicolon of  each item under the each section

   

;%VID_XXXX&PID_XXXX.DeviceDesc%=CyUsb, USB\VID_XXXX&PID_XXXX

   

 Change the VID_XXXX to contain the hexadecimal value of the VendorID for the device

   

 Change the PID_XXXX to contain the hexadecimal value of the ProductID for the device

   

 

   

Change [String] section for Device Description according to the Vendor ID and Product ID. 

   

VID_XXXX&PID_XXXX.DeviceDesc="Cypress USB Generic Driver (3.4.4.00)" 

   

Change the VID_XXXX to contain the hexadecimal value of the VendorID for the device

   

 Change the PID_XXXX to contain the hexadecimal value of the ProductID for the device 

   

 

   

 

   

Regards,

   

Gayathri

0 Likes