Announcements

Learn how to optimise USB-C for your designs at 18 May's USB-C PD Webinar.
Click here to register.

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Anonymous
Not applicable
        Hello,   
I use the AN2131S and want to be able to use the whole available memory the AN2131S has (without any additional RAM-memory). I use µVision3 from Keil and ask for the settings I have to make in the "BL51 locate"-tab of the "Options for target"-dialog.   
I think my problem is solved more or less quickly for someone who is experienced with memory-mapping or how it's called (the thing you do in the "BL51 locate"-dialog):   
I wrote a program, which is based on another, smaller program. I kept the settings of the originally (small) program (see screenshot here:    http://www.loaditup.de/413999.html). But I think through the originally settings in this dialog the used memory is very limited... So I want to ask, what I have to modify on this data to be able to use a maximum of the memory of the AN2131S.   
   
A second question: Are the xdata- and the code-spaces both on the same memory (the XRAM)? And how much XRAM has the AN2131 (I read something about 4k or 8k)?   
   
Regards,   
Stefan   
2 Replies
Anonymous
Not applicable
        AN2131S has 8k RAM... This part is obsolete for a very long time... May i know why you are experimenting with this part???   
This memory is shared by code and data....   
0 Likes
Anonymous
Not applicable
        I am a student, who has built a usb-board with the AN2131 in school... I know, that it is a no longer current device, but i have this board 😉   
0 Likes