- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Sorry for my english.
Controller - cy7c6801 - 56pins.
From the examples I do not understand how you can easily convey the state of input-output ports on the usb in my application. If not hard - give a simple example for learning (very desirable in the C language).
Thanks in advance!
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
The part number that you had mentioned is incomplete. I believe you are using FX2LP (CY7C68013). If so, for using the various IO pins as GPIOs, you can refer section 11.9 in the EZ-USB Technical reference manual, which you can find at " \Cypress\USB\doc\FX2LP " after installing FX2LP DVK (http://www.cypress.com/?rID=14321)
Regards,
Gayathri
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
Thank you - good example..
Yes controller cy7c68013 - 56 Pins
With the transfer of data from the ports figured out.
I can not find an example of software implementation of SPI interface - specifically found only AN14558 document but there is no source projects, and the realization I did not like.
Help? 🙂
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
Thank, but my MCU with 56 pins not have UART interface - i need other example.