- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi
I have a question about the ATA standards supported by theI have a question about CY7C68300C-56LTXC
Qestion1
I use the IF below. Is there a compatibility issue?
・ ATA3
-ATAPI command: Compliant with SFF-8020 Rev2.6 and SFF-8090 Rev0.99 specifications
・ Transfer mode:
PIO mode 0,1,2,3,4
Single Word mode 0,1,2
Multi Word mode 0,1,2
I checked the data sheet, but some modes are not supported.
Should we determine in the system that an unsupported mode is needed?
CY7C68300C-56LTXC datasheet
https://www.cypress.com/file/39151/download
Qestion2
CY7C68300C-56LTXC The following signals are not supported.
・ DASP
・ PDIAG
・ CSEL
Does CY7C68300C-56LTXC support only one ATA device?
Is the above signal unnecessary if there is only one ATA device?
junya
Solved! Go to Solution.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
AT2LP only supports modes listed in the datasheet. Therefore from the set modes, it will use the highest one used by the connected driver.
CY7C68300C-56LTXC supports 2 ATA devices in the configurations mentioned in the datasheet. Please refer to AT2LP RDK schematic for pin connection - https://www.cypress.com/documentation/reference-designs/cy4615b-hi-speed-usb-20-ataatapi-bus-powered...
Pranava
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
AT2LP only supports modes listed in the datasheet. Therefore from the set modes, it will use the highest one used by the connected driver.
CY7C68300C-56LTXC supports 2 ATA devices in the configurations mentioned in the datasheet. Please refer to AT2LP RDK schematic for pin connection - https://www.cypress.com/documentation/reference-designs/cy4615b-hi-speed-usb-20-ataatapi-bus-powered...
Pranava