Mar 16, 2023
03:32 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Mar 16, 2023
03:32 AM
Hello,
In the Device Configuration Utility (Windows only) of USB-Serial Bridge IC, there is a parameter "VBUS Voltage is 3.3 V", and it is explained to check the checkbox when supplying 3.3 V from VBUS to CY65211.
Is it possible to use VBUS 3.3V in the same way in Linux system?
If so, how should I configure it?
As you know, there is no Device Configuration Utility provided for Linux.
MPN: CY65211-24LTXI
Thanks.
Labels
1 Reply
Mar 16, 2023
04:16 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Mar 16, 2023
04:16 AM
Hello,
The device can be configured with USB serial Configuration utility (on Windows) and then can be used on Linux
or
Please refer to this thread for downloading configuration utility (linux) Solved: USB-Serial Configuration Utility source code (CY7C... - Infineon Developer Community
Regards,
Rashi
Rashi
This widget could not be displayed.