Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

USB low-full-high speed peripherals Forum Discussions

Anonymous
Not applicable

 Hi.

   

i have test slavefifo stream test.

   

result data are like this.

   

   

 

   

2 2 3 3 4 4 5 5 6 6 7 7 8 8 9 9 A A B B C C D D E E F F 10 10 11 11 12 12 13 13 14 14 15 15 16 16 17 17 18 18 19 19 1A 1A 1B 1B 1C 1C 1D 1D 1E 1E 1F 1F 20 20 21 21 22 22 23 23 24 24 25 25 26 26 27 27 28 28 29 29 2A 2A 2B 2B 2C 2C 2D 2D 2E 2E 2F 2F 30 30 31 31 32 32 33 33 34 34 35 35 36 36 37 37 38 38 39 39 3A 3A 3B 3B 3C 3C 3D 3D 3E 3E 3F 3F 40 40 41 41 42 42 43 43 44 44 45 45 46 46 47 47 48 48 49 49 4A 4A 4B 4B 4C 4C 4D 4D 4E 4E 4F 4F 50 50 51 51 52 52 53 53 54 54 55 55 56 56 57 57 58 58 59 59 5A 5A 5B 5B 5C 5C 5D 5D 5E 5E 5F 5F 60 60 61 61 62 62 63 63 64 64 65 65 66 66 67 67 68 68 69 69 6A 6A 6B 6B 6C 6C 6D 6D 6E 6E 6F 6F 70 70 71 71 72 72 73 73 74 74 75 75 76 76 77 77 78 78 79 79 7A 7A 7B 7B 7C 7C 7D 7D 7E 7E 7F 7F 80 80 81 81 82 82 83 83 84 84 85 85 86 86 87 87 88 88 89 89 8A 8A 8B 8B 8C 8C 8D 8D 8E 8E 8F 8F 90 90 91 91 92 92 93 93 94 94 95 95 96 96 97 97 98 98 99 99 9A 9A 9B 9B 9C 9C 9D 9D 9E 9E 9F 9F A0 A0 A1 A1 A2 A2 A3 A3 A4 A4 A5 A5 A6 A6 A7 A7 A8 A8 A9 A9 AA AA AB AB AC AC AD AD AE AE AF AF B0 B0 B1 B1 B2 B2 B3 B3 B4 B4 B5 B5 B6 B6 B7 B7 B8 B8 B9 B9 BA BA BB BB BC BC BD BD BE BE BF BF C0 C0 C1 C1 C2 C2 C3 C3 C4 C4 C5 C5 C6 C6 C7 C7 C8 C8 C9 C9 CA CA CB CB CC CC CD CD CE CE CF CF D0 D0 D1 D1 D2 D2 D3 D3 D4 D4 D5 D5 D6 D6 D7 D7 D8 D8 D9 D9 DA DA DB DB DC DC DD DD DE DE DF DF E0 E0 E1 E1 E2 E2 E3 E3 E4 E4 E5 E5 E6 E6 E7 E7 E8 E8 E9 E9 EA EA EB EB EC EC ED ED EE EE EF EF F0 F0 F1 F1 F2 F2 F3 F3 F4 F4 F5 F5 F6 F6 F7 F7 F8 F8 F9 F9 FA FA FB FB FC FC FD FD FE FE FF FF 0 0 1 1 2 2 3 3 4 4 5 5 6 6 7 7 8 8 9 9 A A B B C C D D E E F F 10 10 11 11 12 12 13 13 14 14 15 15 16 16 17 17 18 18 19 19 1A 1A 1B 1B 1C 1C 1D 1D 1E 1E 1F 1F 20 20 21 21 22 22 23 23 24 24 25 25 26 26 27 27 28 28 29 29 2A 2A 2B 2B 2C 2C 2D 2D 2E 2E 2F 2F 30 30 31 31 32 32 33 33 34 34 35 35 36 36 37 37 38 38 39 39 3A 3A 3B 3B 3C 3C 3D 3D 3E 3E 3F 3F 40 40 41 41 42 42 43 43 44 44 45 45 46 46 47 47 48 48 49 49 4A 4A 4B 4B 4C 4C 4D 4D 4E 4E 4F 4F 50 50 51 51 52 52 53 53 54 54 55 55 56 56 57 57 58 58 59 59 5A 5A 5B 5B 5C 5C 5D 5D 5E 5E 5F 5F 60 60 611 1 

   

 

   

Origianlly, i was expected data is like  this 

   

0 1 2 3 4 5 6 ...

   

but i can't it. Why happend this result data?

0 Likes
1 Reply
Anonymous
Not applicable

Can you please let us know which application note example project you used?

0 Likes