Announcements

Learn how to optimise USB-C for your designs at 18 May's USB-C PD Webinar.
Click here to register.

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

lock attach
Attachments are accessible only for community members.
Anonymous
Not applicable

    Hello everyone!

   

    Thank you for your attention!My firmware sets the EP2 as OUT(from PC side) and EP6 as IN. Also, FLAGA shows whether there are data in 2KB FIFO of  EP2, FLAGD shows whether there are data in 2KB FIFO of EP6.  68013A is connected with an FPGA. The FPGA will monitor the state of  FLAGA and read the data, then write back to EP6.

   

    The problem is, I failed to read the data after sent them.  When I download 2KB data to EP2 with CyConsole. FLAGD shows the FIFO of EP6 is full. I continued to download 2KB data to EP2, the FLAGA is set up, too. It means the FIFO of EP2 is full.

   

    I think the path from EP6 to PC is blocked, while the datasheet tells me the 68013A will package the data and send it to PC automatically. Could you help  to find out why? Thank you very much!

   

 

   

    The attachment is captured by USB-Trace when I send 512KB data 4 times, and fail to read 512KB back. 

2 Replies
Anonymous
Not applicable

Hi,

   

Please create a Tech Support case and provide us with the original usbtrace file for our inspection.

   

Regards,

   

- Madhu Sudhan

0 Likes
Anonymous
Not applicable

  OK! Thank you very much! I've created a case. And do you have any guess about the problem with the information I have provided?

0 Likes