Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
Anonymous
Not applicable

 I am trying to write data to EP2 (configured as double buffered OUT in manual mode).

   

For debugging reasons, once the fx2 receives the data, I want it to commit some of the bytes to a packet and send to the host via EP1.

   

Relevant code: lives in a function which is regularly polled 

   

 

   
  if(!(EP2468STAT & 0x01))   {     //EP2EF=0 so not empty     SYNCDELAY();      EP1INBUF[0] = 0x09;     EP1INBUF[1] = EP2FIFOBUF[0];     EP1INBUF[2] = EP2FIFOBUF[1];     EP1INBUF[3] = EP2FIFOBUF[2];     EP1INBUF[4] = EP2FIFOBUF[3];     EP1INBUF[5] = EP2FIFOBUF[4];     EP1INBUF[6] = EP2FIFOBUF[5];     EP1INBUF[7] = EP2FIFOBUF[6];     EP1INBUF[8] = EP2FIFOBUF[7];     EP1INBUF[9] = EP2FIFOBUF[256];     EP1INBUF[10] = EP2FIFOBUF[257];     EP1INBUF[11] = EP2FIFOBUF[258];     EP1INBUF[12] = EP2FIFOBUF[259];     EP1INBUF[13] = EP2FIFOBUF[260];     EP1INBUF[14] = EP2FIFOBUF[261];     EP1INBUF[15] = EP2FIFOBUF[262];     EP1INBUF[16] = EP2FIFOBUF[263];     EP1INBUF[17] = EP2468STAT;     EP1INBC = 18;      SYNCDELAY();     OUTPKTEND = 0x02; //pass on and re-arm   }
   

The data in EP1BUF[17] returns as 0x64 for the first packet, and 0x66 for the second packet sent.

Not sure as to why 0x64 is possible, since the FIFO can't be both full and empty (am I accidently reading it here during a flag change? (This in reproducible behavior though)) Also, any subsequent attempts to read/write to *any* other endpoints timeout, as if the whole device has locked up. Any ideas? Thanks. Ali   
0 Likes
8 Replies
Anonymous
Not applicable

section 1.18 EZ-USB Endpoint Buffers (page 32) contains the allowed endpoint configurations. Most probably you are configuring just EP2 to double buffering and putting the endpoint FIFOs in an unknown state. Configure the endpoint FIFOs to one of the 12 allowed configuration and things should work fine.

   

Regards,

   

Anand 

0 Likes
Anonymous
Not applicable

 In my init function, I configure all 4 EPs, so I don't see why it should be in an unknown state:

   

 

   
  //Slave EPs setup   EP2CFG = 0xA2; SYNCDELAY(); //BULK OUT 512 2x   EP4CFG = 0xA2; SYNCDELAY(); //BULK OUT 512 2x   EP6CFG = 0xE2; SYNCDELAY(); //BULK IN 512 2x   EP8CFG = 0xE2; SYNCDELAY(); //BULK IN 512 2x    //Slave FIFO setup   FIFORESET = 0x80; SYNCDELAY();   FIFORESET = 0x82; SYNCDELAY();   FIFORESET = 0x84; SYNCDELAY();   FIFORESET = 0x86; SYNCDELAY();   FIFORESET = 0x88; SYNCDELAY();   FIFORESET = 0x00; SYNCDELAY(); 
0 Likes
Anonymous
Not applicable

Are you priming the pump for the out endpoints using OUTPKTEND = 0x82 etc, here 2 is the endpoint number of the out endpoint.

   

Better yet can you post your init part of the code here.

   

Regards,

   

Anand

0 Likes
Anonymous
Not applicable

 Sure. The whole user init function:

   

 

   
void init_user() {   EA = 0;    CPUCS = 0x10; //48MHz   IFCONFIG = 0xE3; //INTCLK, 48, DRIVE, SYNC, SLAVE   SYNCDELAY();       //Setup debug endpoints   EP1OUTCFG = 0xB0; SYNCDELAY(); //Interrupt   EP1INCFG = 0xB0; SYNCDELAY();    REARMEP1OUT();    //Setup LED output, and light it   PORTCCFG &= ~0x80;   OEC |= 0x80;    //Slave EPs setup   EP2CFG = 0xA2; SYNCDELAY(); //BULK OUT 512 2x   EP4CFG = 0xA2; SYNCDELAY(); //BULK OUT 512 2x   EP6CFG = 0xE2; SYNCDELAY(); //BULK IN 512 2x   EP8CFG = 0xE2; SYNCDELAY(); //BULK IN 512 2x    //Slave FIFO setup   FIFORESET = 0x80; SYNCDELAY();   FIFORESET = 0x82; SYNCDELAY();   FIFORESET = 0x84; SYNCDELAY();   FIFORESET = 0x86; SYNCDELAY();   FIFORESET = 0x88; SYNCDELAY();   FIFORESET = 0x00; SYNCDELAY();    PINFLAGSAB = 0x98; SYNCDELAY(); //EP2EF, EP4EF   PINFLAGSCD = 0xEF; SYNCDELAY(); //EP6FF, EP8FF   FIFOPINPOLAR = 0x00; SYNCDELAY();     //Manual mode   EP2FIFOCFG = 0x01; SYNCDELAY(); //WW    //Arm the pump   OUTPKTEND = 0x82; SYNCDELAY();   OUTPKTEND = 0x82; SYNCDELAY();    EP6FIFOCFG = 0x00; SYNCDELAY();   EP6FIFOCFG = 0x0D; SYNCDELAY(); //AUTOIN, ZEROLEN, WW   EP8FIFOCFG = 0x00; SYNCDELAY();   EP8FIFOCFG = 0x0D; SYNCDELAY(); //AUTOIN, ZEROLEN, WW   EP6AUTOINLENH = 0x02; SYNCDELAY();   EP6AUTOINLENL = 0x00; SYNCDELAY();   EP8AUTOINLENH = 0x02; SYNCDELAY();   EP8AUTOINLENL = 0x00; SYNCDELAY();    EA = 1; }
This is setup so that I believe EP2 is manual out, and EP6+8 are autoin.   
0 Likes
Anonymous
Not applicable

Hi Ali,

   

Sorry I didn't read the post properly earlier.

   

when the first packet is sent, the buffer is 2 packet wide and it has 1 packet in it so it is neither empty nor full. So 0x64 is a legal value.

   

When you send the second packet, the buffer is 2 packet wide and it has 2 packets so it is full. So 0x66 is the right value. Hope this clears your doubt.

   

Regards,

   

Anand

0 Likes
Anonymous
Not applicable

Hi,aasi

   

why does my FX2LP EP6FF remain high always,which reflected by FLAGB configured in firmware?

   

Appearance:

   

 for(i=0;i<1125;i++)
 {    
  for(j=0;j<512;j++)
  {
   *(Uint8 *)USB_FIFO6_ADDR=iCount;
   while(USB_FLAGB==1);//stopping here always.
  }
  
  iCount++;
  if(iCount==256)
  {
   iCount=0;
  }
 }

   

 

   

 for(i=0;i<1125;i++)
 {    
  for(j=0;j<512;j++)
  {
   *(Uint8 *)USB_FIFO6_ADDR=iCount;
   while(USB_FLAGB==0);//not stopping here ,but some data will be lost  when data be received from pc.
  }
  
  iCount++;
  if(iCount==256)
  {
   iCount=0;
  }
 }

   

why?is FX2LP damaged or my firmware does not configured correctly?

   

i 'm letted be in my casese.

   

thank you.

0 Likes
Anonymous
Not applicable

When EP6 is full you should be reading packets from EP6 for its full flag to de-assert. Is this being done?

0 Likes
Anonymous
Not applicable

Yes,i have readed them out from PC Software.but can't read data because  dsp code stopping in this :

   

while(USB_FLAGB==1);

   

 

   

That is :

   

My FX2LP FLAGB remains High always after reseting or starting.why??

0 Likes