Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

USB low-full-high speed peripherals Forum Discussions

DaBo_288066
Level 2
Level 2

Hi all,

   

Using the "ControlCenter" application available into FX3 SDK I see that a .iic firmware file can be wrote, into a FX2 coupled EEPROM, in a fraction of the time needed for the same operation performed by the old FX2's "ControlCenter". This is very interesting...

   

I understand that this operation is performed by LoadEEPROM function available into the new CyUSB .NET library. But is it possible to implement the same thing in a custom fw/sw? Can you provide the fw/sw source to perform such R/W speedy operations on FX2 coupled EEPROM?

   

Thanks a lot.

0 Likes
1 Reply
Anonymous
Not applicable

Hi,

   

Please contact the Cypress Tech Support for details on the firmware.

   

Regards,

   

- Madhu Sudhan

0 Likes