I have a project that I am developing using the FX2 platform to read an I2C based encoders. The system will host five different encoders which are read by the I2C bus and I would like to read their data buffer and place into a buffer to be read back by the computer when you do a bulk read. This way each transaction on the USB bus yields the buffer contents of all five encoders. I was trying to write the return of EZUSBReadI2C into EP2FIFOBUF but EP2FIFOBUF won't accept the data.
Solved! Go to Solution.
Hi Yatheesh,
I was able to get the firmware to work the way I would like it to. Thank you for the help. To correct the return value changing from the default value to 1 instead of incrementing the default value when the encoder is turned, I added a second programming of the initial values using a EZUSB_WriteI2C(encoder, 17, (WORD)Setup_Data); . Not reala second time. I am not sure why this works but it does. To get the unit to load defaults without a Vendor Request I added if(!(ENCODER_RDY))initialize_encoder(); to TD_Poll(). Now when I plug the unit in the encoders read correctly and there is no need for a vendor request unless you want to reset the default values. Thanks for all the help!
void initialize_encoder()
{
int i, ii, iii;
BYTE Status;
BYTE xdata Setup_Data[17];
WORD Read_Data;
ii = 0;
iii =1;
//Reset the FIFO
FIFORESET = 0x80;
SYNCDELAY;
FIFORESET = 0x02;
SYNCDELAY;
FIFORESET = 0x00;
SYNCDELAY;
//Fill Encoder_Data with Setup contents
for (i=0; i < ENCODER_N; i++){
counter = default_counter;
Setup_Data[0] = 0x00; //Register to Start
Setup_Data[1] = 0x0B; //General Config
Setup_Data[2] = 0x00; //Status
Setup_Data[3] = 0x00; //Counter Byte 4
Setup_Data[4] = 0x00; //Counter Byte 3
Setup_Data[5] = 0x00; //Counter Byte 2
Setup_Data[6] = 0x00; //Counter Byte 1
Setup_Data[7] = 0x00; //Max Byte 4
Setup_Data[8] = 0x00; //Max Byte 3
Setup_Data[9] = 0xFF; //Max Byte 2
Setup_Data[10] = 0xFF; //Max Byte 1
Setup_Data[11] = 0x00; //Min Byte 4
Setup_Data[12] = 0x00; //Min Byte 3
Setup_Data[13] = 0x00; //Min Byte 2
Setup_Data[14] = 0x00; //Min Byte 1
Setup_Data[15] = 0x00; //LED A
Setup_Data[16] = 0x00; //LED B
Setup_Data[5] = MSB(default_counter); //Counter Byte 2
Setup_Data[6] = LSB(default_counter); //Counter Byte 1
EZUSB_WriteI2C(encoder, 17, (WORD)Setup_Data);
EZUSB_WaitForEEPROMWrite(encoder);
EZUSB_WriteI2C(encoder, 17, (WORD)Setup_Data);
EZUSB_WaitForEEPROMWrite(encoder);
Status = Encoder_Status(encoder);
Read_Data = Encoder_Read_Word(encoder, DATA_COUNTER_BYTE2);
counter = default_counter;
if(Read_Data != counter){// && (ENCODER_RDY)){
Encoder_LED(encoder, DECREASE, 500);
}
EP2FIFOBUF[ii] = LSB(Read_Data);
EP2FIFOBUF[iii] = MSB(Read_Data);
ii = ii + 2;
iii = iii + 2;
Encoder_LED(encoder,INCREASE, 50);
}
for (i=10;i<16;i++){
EP2FIFOBUF=0xFF;
}
ENCODER_RDY = TRUE;
}