Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

USB low-full-high speed peripherals

Chris_Hawthorne
Level 3
10 replies posted 10 sign-ins 5 replies posted
Level 3

Can I use a development kit CY3684 to debug the firmware for CY7C68014A-56PVXC?  The development kit uses the CY7C68013A-128AXC which also has access to the serial port  for the KEIL debugger.  I don't need all the functionality of the 128 pin part and the power consumption is also a benefit is the reason to use CY7C68014A-56PVXC

Thanks in Advance!

Chris

0 Likes
1 Solution
YiZ_31
Moderator
Moderator 1000 replies posted 750 replies posted 500 replies posted
Moderator

Hi Chris,

Yes, you can. But you should move your code into the CY7C68014A-56PVXC project after debugging, they are not pin-to-pin devices.

View solution in original post

0 Likes
1 Reply
YiZ_31
Moderator
Moderator 1000 replies posted 750 replies posted 500 replies posted
Moderator

Hi Chris,

Yes, you can. But you should move your code into the CY7C68014A-56PVXC project after debugging, they are not pin-to-pin devices.

0 Likes