CYUSB2014-BZXC: How to sync Input Clock GPIO Pin to an Output GPIO Pin?

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
hershdhami
Level 1
Level 1
First like given First question asked Welcome!

Hello,

I have a 50MHz external clock that is being driven into a GPIO pin on the CYUSB2014-BZXC and was wondering if there was a way to sync this to an output GPIO pin with the BOOT library?

This also raises the question, should I stick with boot or switch to the U3 Library (U3 vs FX3)? I don't necessarily need multithreads or RTOS, but it looks like there is less functionality with boot.

Thanks,

Hersh

0 Likes
1 Solution
1 Reply