Anonymous
Not applicable
Jun 02, 2010
06:41 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Jun 02, 2010
06:41 AM
I have developed a board in which I have used EZ-USB FX2LP dveice CY7C68013A for data transfer from HOST PC to FPGA. I am facing problem in device detection on the host pc (Windows XP). As I connect the USB cable between CPU and the board on the computer there is no notification pop up for deveice detection. When I look into the device manager window the device pannel is getting refreshed continuously. I have checked all the voltage leves required on critical pins thoroughly as per the guideline provided in documents. Please assist in this regard.
1 Reply
Anonymous
Not applicable
Jul 05, 2010
12:01 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Jul 05, 2010
12:01 AM
您好:
我用68013A-100这个芯片,想把端口配置成 ISO 传输模式,可是,配置寄存器EPXCFG之后,用你们的开发工具CONTROL PANNAL 中的GET PIPES,
Pipe: 0 Type: BLK Endpoint: 2 OUT MaxPktSize: 0x200
Pipe: 1 Type: BLK Endpoint: 6 IN MaxPktSize: 0x200
没有找到想要的ISO传输模式的端口,请问这是怎么回事?如何配置,才能正常工作。
谢谢您的浏览,期待您的回复。