CY7C65213 - Internal pull-up/down for SLEEP# and POWER#

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
JuIn_1625121
Level 5
Level 5
100 sign-ins First solution authored 100 replies posted

I think that each SLEEP# and POWER# outputs are connected internally 5.6kohm resistors for pull-up and pull-down.

Is it correct?

pastedImage_0.png

0 Likes
1 Solution
SrinathS_16
Moderator
Moderator
Moderator
1000 replies posted 750 replies posted 500 replies posted

Hello Inoue-san,

- The pull-up/down resistors that you have mentioned refer to the internal pull-up/down.

- When a GPIO is to be used as an output pin, there is no need for an external pull-up/down to be connected.

- When a GPIO is configured as an input pin, there should be a pull-up/pull-down present on the pin so that the pin is in a known state nd not left floating.

Best regards,

Srinath S

View solution in original post

2 Replies
SrinathS_16
Moderator
Moderator
Moderator
1000 replies posted 750 replies posted 500 replies posted

Hello Inoue-san,

- The pull-up/down resistors that you have mentioned refer to the internal pull-up/down.

- When a GPIO is to be used as an output pin, there is no need for an external pull-up/down to be connected.

- When a GPIO is configured as an input pin, there should be a pull-up/pull-down present on the pin so that the pin is in a known state nd not left floating.

Best regards,

Srinath S

Hello Srinath-san,

Thank you for your answer.

I understood it.

Best Regards,

Inoue

0 Likes