Announcements

Learn how to optimise USB-C for your designs at 18 May's USB-C PD Webinar.
Click here to register.

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Anonymous
Not applicable

Hello everybody,

   

i have a CY7C65213-32LTXI chip on my custom board.

   

It should work as a UART interface,

   

but when i connect to it it says it is in  CY_TYPE_MFG mode and no UART SetFunction or even GetConfig will work.

   

 

   

- I tried to program it with "USB Serial Configuration Utility.exe" but it wont change the Device type...

   

- Do i need to program the Flash or what?

   

- even if, where can i get a binary to flash??

   

- or is it just the wrong driver???

   

 

   

tnx in advance

5 Replies
Anonymous
Not applicable

Hi,

   

 

   

Can you create a tech support case at https://secure.cypress.com/myaccount/?id=25&createCase=techSupport with screenshot of  "USB Serial Configuration Utility.exe" when device is connected?

   

-Haneesh

0 Likes
Anonymous
Not applicable




   

Ok, heres the screens from the Config tool. This is using a little Evalboard not the custom boar but i have the same Error with the API that i cannot get the uart config or even set.

   

many tnx in advance

   

 

   

 

   

0 Likes
lock attach
Attachments are accessible only for community members.
Anonymous
Not applicable

Does it work now?

   

Dammit spam filter..

0 Likes
spa_rika
Level 1
Level 1
5 sign-ins First reply posted First question asked

Hello,

I have this exact same problem now. Has this been solved?

0 Likes
Meghavi
Moderator
Moderator
Moderator
250 replies posted 100 solutions authored 10 likes received

Hi,

If the device is configured as UART under CDC mode, then the device type will be returned as CY_TYPE_MFG. Please set the protocol as Vendor mode in USB Serial Configuration Utility for CY_TYPE_UART.

Regards

0 Likes